About Logic Gates

You can add logic gates to the Logic Tree to define a connection between nodes. A logic gate is defined in an RCA Logic Gate and is represented in the Logic Tree by a Logic Gate node. You can use Logic Gate nodes to add Boolean logic between nodes (i.e., AND and OR statements). The AND Logic Gate is represented by the The AND gate symbol in the Logic Tree. The OR Logic Gate is represented by the The OR Gate symbol in the Logic Tree.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.