RCA Analysis record store basic information about a Root Cause Analysis created to track and analyze causes of Asset failures. The following table provides an alphabetical list and description of the fields that exist for the Root Cause Analysis family and appear by default on the RCA Analysis, RCA Analysis Summary, and Plant & Equipment Info datasheets. The information in the table reflects the baseline state and behavior of these fields. This list is not comprehensive.
Note: The fields available on the Plant & Equipment Info datasheet exist in the Definition section on the Analysis Summary workspace so that you can view this information in analyses where it existed in previous releases. In the current product, the Linked Assets tab in the Analysis Summary workspace allows you to link Assets to the Root Cause Analysis.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
Field | Data Type | Description | Behavior |
---|---|---|---|
Analysis Name |
Character |
A value that identifies the Root Cause Analysis throughout the Meridium Enterprise APM product. |
This is a required field, and it must be unique. |
Analysis Type |
Character |
The type of RCA you are conducting. |
This field contains a list of the following values:
You can select the value that defines the type of analysis you are performing. This field is available on the RCA Analysis and RCA Analysis Detail datasheets only. |
Asset Category |
Character |
The category of equipment associated with the RCA. |
You can enter a value in this field to describe the Asset identified in the Asset ID field. This field is labeled Equipment Category on the datasheet. This field is available on the Plant & Equipment Info datasheet only. |
Asset Class |
Character |
The class of equipment associated with the RCA. |
You can enter a value in this field to describe the Asset identified in the Asset ID field. This field is labeled Equipment Class on the datasheet. This field is available on the Plant & Equipment Info datasheet only. |
Asset ID |
Character |
A unique value that identifies the piece of equipment on which the analysis is being performed. |
You can enter in this field the name of the Asset you are analyzing. This field is labeled Equipment ID on the datasheet. This field is available on the Plant & Equipment Info datasheet only. |
Asset Type |
Character |
The type of equipment associated with the RCA. |
You can enter a value in this field to describe Asset identified in the Asset ID field. This field is labeled Equipment Type on the datasheet. This field is available on the Plant & Equipment Info datasheet only. |
Charter |
Text |
The purpose of and requirements associated with conducting the RCA. |
This field is available only after you have entered a Team Charter in the Team Charter section. This value is populated automatically with the charter that you entered in the Team Charter section. |
Comments |
Text |
Any additional information about the current analysis. |
You can enter comments in this field. |
Cost |
Number |
The estimated cost of the failure event(s) you are analyzing. By default, the currency is set to $. |
You can enter a value in this field to specify the estimated cost. |
Date Published |
Date |
The date on which the RCA was published. |
This field is disabled. When the RCA is published, this field is updated automatically with the published date. |
Division |
Character |
The division of the equipment on which the RCA is being performed. |
You can enter a value in this field to describe the piece of equipment identified in the Asset ID field. This field is available on the Plant & Equipment Info datasheet only. |
End Date |
Date |
The end date of the analysis, if applicable. |
You can select a date using the Calendar tool. The date specified in the End Date field must be greater than the date specified in the Start Date field. |
Event Narrative |
Text |
Information about the equipment failure. |
You can enter a description of the event in this field. |
Frequency |
Number |
The number of times the equipment failure occurred. |
You can enter a value in this field. |
Functional Location |
Character |
The location containing the piece of equipment on which you are performing the RCA. |
You can enter the name of the location that you are analyzing in this field. This field is available on the Plant & Equipment Info datasheet only. |
Long Description |
Text |
A brief description of the current RCA. |
You can enter text in the Analysis Description dialog box. This field is labeled Analysis Description on the datasheet. |
Manufacturer |
Character |
The manufacturer of the piece of equipment on which you are performing the analysis. |
You can enter a value in this field to describe the manufacturer of the Asset identified in the Asset ID field. This field is available on the Plant & Equipment Info datasheet only. |
Plant Location |
Character |
The plant where the equipment failure occurred. |
You can enter a value in this field to describe the plant location of the asset identified in the Asset ID field. This field is available on the Plant & Equipment Info datasheet only. |
Start Date |
Date |
The start date of the analysis. |
You can select a date using the Calendar tool. |
Unit |
Character |
The ID of the unit where the piece of equipment for which you are conducting the RCA exists. |
You can enter a value in this field to describe the unit of the asset identified in the Asset ID field. This field is available on the Plant & Equipment Info datasheet only. |
Copyright © 1993-2016 Meridium, Inc. All rights reserved.