About Access to Configuration Manager Features

You need a Developers license to perform the following functions:

The following table lists the permissions granted to the to the MI Configuration Role and MI APMNow Admin Security Groups for accessing the various administrative features of Configuration Manager.

Feature Permission Notes
Security Group: MI Configuration Role
Entity Family Add, Edit, or Delete  
Fields Add, Edit, Delete  
Field Behavior Add, Edit, or Delete  
Relationship Family Add, Edit, or Delete  
Relationship Definitions Add, Edit, Delete  
Datasheet Add, Edit, or Delete  
State Configuration Add, Edit, or Delete  
Family Reports (Associate SSRS Reports) Add, Edit, or Delete  
Associated Pages Add, Edit, or Delete  
Family Policies Add, Edit, or Delete  
System Codes and Tables Add, Edit, or Delete  
Units of Measure and Conversions Add, Edit, or Delete  
Manage Translations Not Applicable There is no add, edit, or delete function that you can perform in this feature. However, if you are a part of this group, then you can perform all of the translations tasks.
Import Not Applicable There is no add, edit, or delete function that you can perform in this feature. However, you can import all metadata if you are part of this group.
Export Not Applicable There is no add, edit, or delete function that you can perform in this feature. However, you can export metadata if you are part of this group.
Content Validation Not Applicable There is no add, edit, or delete function that you can perform in this feature.
Security Groups: MI APMNow Admin
Associated Pages Add, Edit, or Delete  
Datasheet Add, Edit, or Delete

 

Family Reports Add, Edit, or Delete There is no edit function that you can perform on this feature. However, you can mark a report as default.
Field Edit  
Field Behavior Edit  
Family Policies Add, Edit, or Delete  
State Configuration Add, Edit, or Delete  
System Codes and Tables Add, Edit, or Delete  
Units of Measure and Conversions Add, Edit, or Delete  

Note: The other features of Family Management are not available for the MI APMNow Admin group. The Import and Export features are also not available to the MI APMNow Admin group.

Copyright © 1993-2017 Meridium, Inc. All rights reserved.