This topic describes how to access the datasheet of the following types of components of a hazards analysis:
Steps
Select the Hazards Worksheets tab.
The Hazards Worksheets section appears, displaying a hierarchical view of the components (Deviations or What Ifs, Causes, Consequences, and Safeguards) associated with the System/Node.
Select the component that you want to access, and then, in the upper-left corner of the workspace, select
The datasheet for the selected component appears.
If needed, modify values in the available fields for Deviation, What If, Cause, Consequence, or Safeguard.
Hint: You can modify a Component only if the corresponding Hazards Analysis is in the Planning state.
In the upper-right corner of the datasheet, select
The changes made to the component are saved.
Tip: You can select
Copyright © 2017 General Electric Company. All rights reserved.