Access a System/Node

Steps

  1. Access the Hazards Analysis that is linked to the System/Node that you want to access.
  2. In the left pane, select the System/Node that you want to access.

    Hint: You can also filter and search for the System/Node by selecting .

    The datasheet for the selected System/Node appears.

    The System/Node datasheet

  3. As needed, modify values in the available fields.

    Hint: You can modify a System/Node only if the corresponding Hazards Analysis is in the Planning state.

  4. In the upper-right corner of the datasheet, select .

    The changes made to the System/Node are saved.

Copyright © 2017 General Electric Company. All rights reserved.