Create a Component

This topic describes how to create the following components of a hazards analysis using a blank datasheet:

You can also copy a Component.

Hint: You can create a Component only if the corresponding Hazards Analysis is in the Planning state.

Steps

  1. Access the System/Node for which you want to create a component.
  2. Select the Hazards Worksheets tab.

    The Hazards Worksheets section appears, displaying a hierarchical view of the components (Deviations or What Ifs, Causes, Consequences, and Safeguards) associated with the System/Node.

    Hazards Worksheet

  3. In the hierarchical level that corresponds to the component that you want to create, select , and then select Create New <type of the component>.

    Where <type of component> can be one of the following values:

    For example, if you want to create a new Deviation, then in the Deviations hierarchical level, select , and then select Create New Deviations.

    A blank datasheet for the type of component appears.

    The blank datasheet of a Deviation

  4. As needed, enter values in the available fields for Deviation, What If, Cause, Consequence, or Safeguard.
  5. In the upper-right corner of the datasheet, select .

    A new component is created and listed in the corresponding hierarchical level. For example, if you have created a new Deviation, it will be listed in the Deviations hierarchical level.

What's Next?

Copyright © 2017 General Electric Company. All rights reserved.