You can link only one asset (one Equipment and one Functional Location) to a Cause or a Safeguard. If an asset is already linked to the Cause or the Safeguard and you link another asset, only the latter one is linked to the Cause or the Safeguard.
Hint: You can link an asset to a Cause or a Safeguard only if the corresponding Hazards Analysis is in the Planning state.
Steps
Access the Cause or the Safeguard that you want to link to an Asset.
The datasheet for the selected Cause or Safeguard appears. The following image shows the datasheet for a Cause.
image
If you want to link an Equipment, follow these steps:
On the datasheet, in the Equipment ID box, select
The Asset Finder window appears.
Navigate to the Equipment that you want to link to the Cause or Safeguard, and then select
In the right pane of the Asset Finder window, the selected Equipment appears .
Select Done.
The Equipment is linked to the Cause or the Safeguard.
Note: When you link an Equipment to the Cause or Safeguard, the Functional Location to which the Equipment belongs is automatically linked to the Cause or Safeguard, and appears in the Functional Location ID box on the datasheet.
If you want to link a Functional Location, follow these steps:
In the Functional Location ID box on the datasheet, select
The Asset Finder window appears.
Navigate to the Functional Location that you want to link to the Cause or Safeguard, and then select
In the right pane of the Asset Finder window, the selected Functional Location appears.
Select Done.
The Functional Location is linked to the Cause or the Safeguard.
Results
What's Next?
Copyright © 2017 General Electric Company. All rights reserved.