Hypothesis nodes are always on the third level of the tree or later, attached either to a Failure Mode node or another Hypothesis node. After you have created the Failure Event node and the Failure Mode nodes, you can add Hypothesis nodes to the Failure Mode nodes and Hypothesis nodes as needed to help the team determine the cause of the event.
This topic describes how to create a Hypothesis on the design canvas. You can also import an existing Hypothesis, copy a Hypothesis, or add a Hypothesis node from the Hypothesis list.
Steps
Use the drag-and-drop method to add the Hypothesis to the Failure Event node or to another Hypothesis on the design canvas.
A new Hypothesis is added and the Properties window appears, displaying the datasheet for the selected Hypothesis.
Select
The Hypothesis appears in the Logic Tree diagram.
Results
What's Next?
Copyright © 2017 General Electric Company. All rights reserved.