Jump to main content
https://www.gevernova.com/
  Products      Documentation      Support          
×

Supercharge your Proficy solution!  Download a free trial of Proficy Operations Hub, CSense analytics, and more. Explore our Proficy 2024 releases!

  1. Home
  2. MQTT Client
  3. Configuration
  4. MQTT Client in Configuration Hub

    Configuration Hub allows you to manage the MQTT Client connections to multiple broker(s) that collect, store, and retrieve data parameters.

  5. MQTT Client Configuration

    Use the following steps to configure the MQTT connections in the Configuration Hub.

  • Version 2024
  • Version 2023
  • Release Notes
  • MQTT Client
    • Getting Started
    • Utilities
    • Configuration
      • MQTT Client in Configuration Hub

        Configuration Hub allows you to manage the MQTT Client connections to multiple broker(s) that collect, store, and retrieve data parameters.

        • MQTT Client Configuration

          Use the following steps to configure the MQTT connections in the Configuration Hub.

          • Manage Identity Providers, Groups, and Users

            By default, the username ch_admin is created in the Proficy Authentication server after registering MQTT Client with the Configuration Hub server. For the first time, you can log in to the Configuration Hub user interface using this username (the password will be the same as the Proficy Authentication secret). After you log in to Configuration Hub, as an administrator, navigate to Proficy Authentication > Security. Depending on the groups assigned to the user, the user will have permissions to access the MQTT client configuration.

          • MQTT Groups in Proficy Authentication

            Proficy Authentication provides group membership access for MQTT clients, such that the users can access the MQTT client configuration from Configuration Hub and read/write OPC UA data.

          • Add MQTT Server for Broker Connection

            MQTT Plugin for Broker connections are edited in the DETAILS section. After selecting a server configuration in the Connections panel, the DETAILS section populates the broker details such as server details, reconnect parameters, and so on.

          • Add Subscriptions to Broker Connection

            Subscriptions are created under the Broker(s) to subscribe to the data parameters.

          • Add Tags to Subscription

            For a Subscription, a Tag is added to load the subscribed MQTT data. Data stored in the tags will be translated from MQTT to OPC UA when the data is published.

          • Secure Connection with Broker

            To establish a secure connection with the MQTT broker, you must import the broker certificate and trust the certificate. This encrypts the data and keeps the broker connection data secure and authenticated.

        • Save and Publish

          When the MQTT node is plugged-in with Configuration Hub, the common toolbar will contain the Save button at the top left. Changes made in Configuration Hub for MQTT nodes are not saved on the server until the changes are published. Until then, any changes are stored in a separate directory on the node being configured.

        • Publish Log and Version

          After you publish the MQTT plugin changes, you can directly view the published log reports by clicking the icon.

        • OPC UA

          The OPC UA protocol is a standard communication mechanism for transferring data between interfaces. OPC UA clients connect to the OPC UA server and collect data from UA Variables.

MQTT Client Configuration

Use the following steps to configure the MQTT connections in the Configuration Hub.

  1. Manage Identity Providers, Groups, and Users.
  2. Add MQTT Server for Broker Connection.
  3. Add Subscriptions to Broker Connection.
  4. Add Tags to Subscription.

Accessibility       Terms        Security        Cookies        Privacy

©2025 GE Vernova and/or its affiliates. All rights reserved.

GE is a trademark of General Electric Company and is used under trademark license.