Upgrade

Upgrade the APM Connect Base to V3.0.2

About This Task

The following table outlines the steps that you must complete to upgrade this module to V3.0.0.

These tasks may be completed by multiple people in your organization. However, we recommend that the tasks be completed in the order in which they are listed.

Note: As of the version of APM Connect released in the first quarter of 2019, you must keep these considerations in mind:
  • Because of changes to the Test Connection function, the CMMS_ID and the System Name in the EAM System record must be the same. Before upgrading, make sure you update the EAM System record so these values match.
  • If you are using multiple cultures from a single source system, existing data must be updated before you upgrade.
  • If you are updating from a significantly older APM Connect version that uses RunDataLoadersRoute.jar or StageDataLoaderService.jar, remove both files.

Procedure

Upgrade from any version V1.0.0 through V2.0.0 to APM Connect Base V3.0.0 and above

  1. Uninstall APM Connect.
  2. Complete the steps to deploy the APM Connect Base for the first time.
    Note: For information about the APM Connect versions corresponding to APM versions, refer to the APM Connect Version Compatibility Table.