Upgrade

Upgrade from any version V5.1.0.0.0 through V5.1.4.1.0

This module will be upgraded to V5.1.5.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.

If an error occurs, delete the following folders:
  • C:\Program Files (x86)\InstallShield Installation Information\<UUID>
  • C:\Meridium\temp

Upgrade from any version V5.0.1.0.0 through V5.0.7.0.0

This module will be upgraded to V5.1.5.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.

If an error occurs, delete the following folders:
  • C:\Program Files (x86)\InstallShield Installation Information\<UUID>
  • C:\Meridium\temp