General Reference
Advanced Visualization Terms
The following terms and definitions apply to advanced visualization dashboard components.
- Chart
- An individual visualization of data using a data source.
- Data Source
- A repository that contains the data that can be visualized in advanced visualization in the form of charts or reports.
- Page
- A collection of charts that can be combined to create a view like a dashboard. These pages can be shared with other users or used as private dashboards for the users
- Domain
- The workspace to create visualizations, where the tenant can configure their own custom data sources. The data sources can be used to access the data and combine that data with the other data that the tenants have access to through the baseline domain that cannot be modified by the users.
- Folders
- A way to organize data in a user domain. This can be used to create various types of content and then saved in different folders that the users can access later.
Advanced Visualization Security Groups
The following table lists the baseline Security Groups available for users within this module, as well as the baseline Roles to which those Security Groups are assigned.
| Role | Group | Role Privileges |
|---|---|---|
| View Advanced Visualization | Everyone | Allows you to view the visualizations that have been created and which other users have shared. |
| Create Advanced Visualization | Create ADV | Allows you to create new visualizations based on the data sources that are available. |
| Manage Advanced Visualization | Manage ADV | Allows you to add new connections or modify existing data connections other than the baseline content that cannot be updated. |
Log Files Collection
Procedure
Start or Stop Advanced Visualization Services
Procedure
Import Content
Procedure
Set APM Host URL
Procedure
Set Reverse Proxy on the APM Host Machine
Procedure
Install IIS Extension on the APM Host Machine
Procedure
- Copy files <Install_DIR>\utils\install_iis_extensions.bat and <Install_DIR>\utils\install_iis_extensions.ps1 from the Advanced Visualization machine to the APM host machine.
- Run the script using one of these methods: