Jump to main content
GE Vernova
  1. Home
  2. Generation Availability Analysis
  3. Reference
  4. Fields that can be Populated from one of the Three Related Records
  • Generation Availability Analysis
    • Overview
    • Workflows
    • Primary Events
    • Contributing Events
    • Related Events
    • Performance Records
    • Manage Root Cause Analysis (RCA) from GAA
    • Manage Log Entries from GAA
    • Reports
    • Admin
    • Data Loaders
    • Deployment and Upgrade
    • Reference
      • General Reference
      • Family Field Descriptions
      • Catalog Items
      • Mappings
      • Allowable Event Types in Related Events
      • Fields that can be Populated from one of the Three Related Records
      • Fuel Code Fields
      • Fuel Information Fields
      • Inactive Hours Field
      • Overlapping between an Outage Event and a Derate Event
      • Capacity Event Types Affecting Performance Records

Fields that can be Populated from one of the Three Related Records

Fields that can be Populated from one of the Three Related Records

When you create a Primary Event record, you will specify, in the Unit ID field, the Unit ID of the GAA Unit record to which the Event record will be linked. When you save the Primary Event record, the APM system will attempt to populate various fields in the Event record with values based on the Unit ID value. These values will not necessarily come directly from the GAA Unit record itself.

  1. First, the APM system will attempt to populate each field with the corresponding value in the Performance record that is linked to the specified GAA Unit record for the month in which the event occurred.
  2. If the associated Performance record does not exist or does not contain a value in a given field, the APM system will attempt to populate the field with the corresponding value in the GAA Unit record.
  3. If the GAA Unit record does not contain a value in a given field, that field will not be populated automatically.

Note that:

  • These fields are populated automatically only when a Primary Event record is first created. After the record exists, the Unit ID field is disabled. Since this value cannot be modified, these fields will never be updated automatically.
  • Fields in new Contributing Event records are populated using these same rules. In other words, fields in Contributing Event records will not necessarily be populated with the same values that exist in the Primary Event record. Instead, they will be populated with the values that exist in the Performance and GAA Unit record at the time the Contributing Event record is created.

The following tables provides a list of fields in Event records that are populated in this way and specifies the corresponding fields in Performance and GAA Unit records that will be used to populate them.

Event RecordPerformance RecordGAA Unit Record
Cause Code GADS Unit Code GADS Unit Code
GADS Unit Type Unit Type Unit Type
GADS Utility Code GADS Utility Code GADS Utility Code
Gross Dependable Capacity Gross Dependable Capacity (G) Gross Dependable Capacity
Gross Maximum Capacity Gross Max Capacity (G) Gross Maximum Capacity
Net Dependable Capacity Net Dependable Capacity (N) Net Dependable Capacity
Net Maximum Capacity Net Maximum Capacity (N) Net Maximum Capacity
Unit Name Unit Name Unit Name
On this page
  • Fields that can be Populated from one of the Three Related Records
© 2025 GE Vernova and/or its affiliates. All rights reserved. GE and the GE Monogram are trademarks of General Electric Company used under trademark license.

Privacy | Terms | Cookies | Accessibility