Reports Upgrade
Upgrade or Update Reports to V5.2.2.0.0
The following table provides you the reference to procedures to upgrade from an earlier APM version to the latest version.
Upgrade from | Upgrade to | Procedure |
---|---|---|
V5.2.x | V5.2.2.0.0 | |
V5.1.x | V5.2.2.0.0 | |
V5.0.x | V5.2.2.0.0 | |
V4.6.2 or a later V4.6.x release | V5.2.2.0.0 | |
V4.6.1.x or earlier | V5.2.2.0.0 |
Note: For more information on upgrading to APM V4.6.2.0.0 or a later V4.6.x release, refer to the Upgrade documentation for the corresponding version.
|
Upgrade from any version V5.2.0.0.0 through V5.2.1.0.0
This module will be upgraded to V5.2.2.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.
Upgrade from any version V5.1.0.0.0 through V5.1.4.0.0
The following tables outline the steps that you must complete to upgrade this module to V5.2.2.0.0. These instructions assume that you have completed the steps for upgrading the basic APM system architecture.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Step | Task | Notes |
---|---|---|
1 | Revert the following queries to baseline to have new section in the NR13 reports:
| This step is required only if you have previously modified the queries. |
Upgrade from any version V5.0.1.0.0 through V5.0.7.0.0
This module will be upgraded to V5.2.2.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.
Upgrade from any version V4.6.2.0.0 through V4.6.11.0.0
This module will be upgraded to V5.2.2.0.0 automatically when you upgrade the components in the basic APM system architecture. No additional steps are required.