Serialization Scheme
Serialization Scheme
Javascript Object Notation (JSON) is the only serialization scheme supported.
The Javascript language does not fully support signed 64-bit integers at the upper and lower value limits. DTO properties defined as type object that have a signed 64-bit integer value are deserialized as string. For example, RowsetDTO.RowValueDTO.ColumnValue.
For JSON serialization:
- Numeric and Boolean values are unquoted.
- Strings are quoted.
- Dates are quoted and are assumed to to be in the time zone of the API authenticated user if not explicitly qualified as a field.
- Dates must be in the
yyyy-MM-ddTHH:mm:ss.fffformat. In this format, the following literal values and required:- Hyphen (-)
- Colon (:)