Elasticsearch Installation
Install Elasticsearch on a Dedicated Server
Procedure
- Download the latest ZIP file for Windows, ElasticSearch 8.17.x, from the official Downloads page.
- Extract the contents of the zip file to C:\ElasticSearch.
- Go to C:\ElasticSearch\elasticsearch-<version>\config, and then access the elasticsearch.yml file.Here, <version> is the version number that you downloaded.
- In the .yml file, uncomment the following properties, and then modify the values to match those shown here:
cluster.name: apm-cluster node.name: ${COMPUTERNAME} path.data: /ProgramData/Meridium/ElasticSearch path.logs: /ProgramData/Meridium/Logs bootstrap.memory_lock: true network.host: 0.0.0.0 http.port: 9200 action.destructive_requires_name: true - For a single node cluster, add the following line of code to the file:
discovery.type: single-node - For a cluster, see https://www.elastic.co/guide/en/elasticsearch/reference/8.17/modules-discovery.html.
- Save and close the .yml file.
- Select the Start button on Windows, right-click Command Prompt, and then select Run as administrator.The Command Prompt window appears.
- At the command prompt, enter cd C:\ElasticSearch\elasticsearch-<version>\bin, and then press Enter.Here, <version> is the version number that you downloaded.
- By default, ElasticSearch is installed with authentication enabled. Follow these steps to set a password for the elastic user.
- At the command prompt, enter elasticsearch-keystore add "bootstrap.password".
- Enter the password.
- By default, ElasticSearch installs with SSL enabled using a self-signed certificate.
- Follow encrypt http communication to use a trusted certificate.
- Or, add this to the elasticsearch.yaml file to turn off SSL xpack.security.http.ssl.enabled: "false"
- At the command prompt, enter elasticsearch-service install, and then press Enter.Elasticsearch is installed.
- Access the Microsoft Management Console (services.msc) and perform the following operations for the Elasticsearch service:
- Verify that the service runs as Local System.
- Modify the startup to be Automatic.
- Start the service to verify installation and configuration.
- On the server on which Elasticsearch is installed, go to http://localhost:9200/ in a web browser. Use “http” if SSL is turned off. Use “elastic” as the username and the password that you set above. Ensure that Elasticsearch runs successfully.A response that is similar to the following sample appears.
{ "name" : "elasticsearch-svr ", "cluster_name" : "docker-cluster", "cluster_uuid" : "o8-U13fNQYCl3K5mCFtduA", "version" : { "number" : "8.17.0", "build_flavor" : "default", "build_type" : "docker", "build_hash" : "2b6a7fed44faa321997703718f07ee0420804b41", "build_date" : "2024-12-11T12:08:05.663969764Z", "build_snapshot" : false, "lucene_version" : "9.12.0", "minimum_wire_compatibility_version" : "7.17.0", "minimum_index_compatibility_version" : "7.0.0" }, "tagline" : "You Know, for Search" } - On the server on which Elasticsearch is installed, go to http://[elastic-search-server]:9200/ in a web browser, and ensure that Elasticsearch runs successfully. A response that is similar to the sample provided in the previous step appears.
- On the APM server, go to C:\ProgramData\Meridium\appsettings.Global.json.
- As needed, modify the following value. Replace localhost with the IP address or the host name of the ElasticSearch Server if it is installed on a separate server.
"elasticSearch": { "url": "http://localhost:9200", "password": "<value>" }, - After all third-party services are configured, reset IIS and services on all APM App Servers.
What To Do Next
Add User Authentication for Elasticsearch
To enhance security, you can implement user authentication for Elasticsearch using the X-Pack security.
Procedure
- From the Elasticsearch installation folder, navigate to the config folder, and then access the file elasticsearch.yml.
- In the .yml file, add the following line of code:
xpack.security.enabled: true - Based on your Elasticsearch cluster type, complete one of the following steps:
- For a single node cluster, add the following line of code in the elasticsearch.yml file:
discovery.type: single-nodeSave and close the elasticsearch.yml file.
- For a multi-node cluster, Elasticsearch requires TLS communication between the nodes. For instructions, refer to https://www.elastic.co/guide/en/elasticsearch/reference/7.9/configuring-tls.html#node-certificates.
- For a single node cluster, add the following line of code in the elasticsearch.yml file:
- From the Elasticsearch installation folder, set the bootstrap password. To do so:
- Run the command prompt as an administrator.
- Change the directory to the Elasticsearch installation folder.
- Run the following command: bin/elasticsearch-keystore add "bootstrap.password"
- Enter the password.
- On the APM server, navigate to C:\ProgramData\Meridium, and then modify the appsettings.Global.json file to update the Elasticsearch settings with the password:
"elasticSearch": { "url": "http://localhost:9200", "password": "<value>" }, - Restart Elasticsearch, Search, and IIS.