Data Collection
About Data Collection
To collect data in the Rounds Data Collection module, you must first access a Route in the RDC Overview page by selecting it in the Overdue Items or Due Items section, or by scanning the barcode of an asset or location. You can then provide readings for Measurement Locations or Lubrication Requirements, as well as create recommendations based on these readings. If geolocation services are enabled, geolocation data will be saved automatically. After you have completed taking readings on a Route, you can mark it done through one of several methods.
About the Route Progress Bar
To indicate the progress a user makes while entering readings on a Route, Rounds Data Collection displays a progress bar indicating the percentage of a Route for which you have entered readings as well as the number of Checkpoints for which you have entered readings on a Route.
This progress bar appears in the following places:
- In the Route Map pane
- In the RDC Overview page, in the Overdue Items and Due Items sections
This progress bar tracks only the progress of an individual user on a specific device for a given Route. In other words, the progress bar does not take into account any activity that occurs on that route by other users on other devices.
A Route with 60 Checkpoints
Consider a Route with 60 Checkpoints that uses Route Scheduling. Assume that two users download the same route. Both users will see the route with 60 checkpoints. If the first user collects 30 readings, they will see their progress bar at 50%. If user 2 collects 45 readings, they will see their progress bar at 75%. The Progress Bar for a route on a device is not aware of other users working on the route.
Consider the same 60 Checkpoint route that uses Checkpoint Scheduling. If one user downloads this route and enters 15 readings on their device, the progress bar for that user on that device for that route will indicate that the Route is 25% complete. The first user uploads and marks the route done, leaving 45 checkpoints still due. If a second user then downloads the same route, this second user does not see that the Route is 25% complete. Instead, this user sees that there are 45 Checkpoints remaining on the Route, and 0% of those 45 Checkpoints have been completed.
About Barcode Scanning
- Improves asset management
- Improves efficiency as barcodes eliminate manual input of data
- Improves processes and streamlines tasks
To use barcode scanning, you should verify that the barcode type that you want to use is currently supported by the APM mobile application. You should also validate that your physical barcodes are compliant with the recommended dimensions and specifications for that type of barcode.
| Barcode Type | Android | iOS | Windows |
|---|---|---|---|
| QR_CODE Note: This barcode type is recommended based on performance and accuracy. | Yes | Yes | Yes |
| DATA_MATRIX | Yes | Yes | Yes |
| UPC_A | Yes | Yes | Yes |
| UPC_E | Yes | Yes | Yes |
| EAN_8 | Yes | Yes | Yes |
| EAN_13 | Yes | Yes | Yes |
| CODE_39 | Yes | Yes | Yes |
| CODE_93 | Yes | Yes | Yes |
| CODE_128 | Yes | Yes | Yes |
| CODABAR | Yes | No | Yes |
| ITF | Yes | Yes | Yes |
| RSS14 | Yes | No | Yes |
| PDF_417 | Yes | Yes | Yes |
| RSS_EXPANDED | Yes | No | No |
| MSI | No | No | Yes |
| AZTEC | Yes | Yes | Yes |
- Use barcodes that have a length of up to 20 characters.
- Barcode scanning is dependent on the camera resolution of the mobile devices and on the condition of the printed barcode.
About Geolocation Data for Readings and Recommendations
If geolocation services are enabled on a device, relevant geolocation data will be saved automatically when you provide readings or create a recommendation.
Accessing Geolocation Data
You can view the geolocation data that is saved for readings, recommendations, and photos via a Map query delivered in the baseline APM catalog.
Availability of Geolocation Data
Location data will be stored only if geolocation services are able to obtain coordinates. This is contingent on the user having granted permission for the APM website or application to access geolocation services on the device in use. In addition, geolocation services may be intermittent; if the geolocation service does not provide a valid response, no location information will be saved to the database.
Accuracy of Geolocation Data
In general, for horizontal location detection when using GPS-based location services (that is, when outdoors and using a smartphone or tablet with built-in GPS), there is >95% probability of the location being accurate within 3.5 meters.
If geolocation is inferred from IP network address, wi-fi, or a cell location, it may be significantly less accurate. For example, if using a browser, geolocation will be inferred from the IP address and wi-fi based location information. At best, a browser is only able to isolate location to a 3 to 5 mile radius, though it could be significantly less accurate. If you are accessing the internet via a corporate network, it is possible that the exposed IP address may imply a different location, possibly even a different country, than where you are physically located.
Access a Route for Data Collection
This topic describes how to access a Route from the RDC Overview page.
Before You Begin
- To access a Route for data collection, the Route must be due or overdue.
- If you want to take readings while offline, the Route must be enabled for offline access and downloaded to the device.
About This Task
Procedure
What To Do Next
About Small Screen Devices
To enhance data collection on small screen devices, such as mobile phones and small tablets, APM automatically adjusts the page layout when you use Rounds Data Collection in portrait mode on any device with a screen less than 769 pixels wide. Regardless of the screen width of your device, the page layout of Rounds Data Collection switches between portrait and landscape modes when you rotate your device, enabling devices with a screen less than 769 pixels wide to use the original page layout when in landscape mode.
Supported Features on Small Screen Devices
The following features are not supported in Rounds Data Collection on small screen devices:
- Selecting an asset name at the top of the workspace for a Route to view the health summary information for that asset in Asset Health Manager.
- Selecting the reading date/time in the in the Measurement Trend graph section of the workspace for a Measurement Location to view the Health Source page.
All other standard features of Rounds Data Collection are supported on small screen devices.
While the supported features behave in the same way when you are using a small screen device as they do when you are using a larger device, the following features are displayed differently:
- The RDC Overview page
As shown in the following image, the contents of the page are adjusted to fit a small screen device.

- The barcode scanner
On a small screen device, the button you select to open the barcode scanner (
) appears in the upper-right corner of a Route and of the RDC Overview page, as shown in the following image. - The Device Settings window
On a small screen device, the button you select to open the Device Settings window (
) appears in the upper-left corner of the RDC Overview page page. Within the Device Settings window, buttons rather than drop-down list boxes appear in the Download Horizon and Sync Interval sections. Additionally, the Scan Option section does not appear on a small screen device. The following image shows the Device Settings window on a small screen device.
- The Route Map pane
On a small screen device, the Route Map pane does not appear automatically when you access a Route for data collection. The button you select to view the Route Map pane (
) appears in the upper-left corner of the workspace for a Route. The Route Map pane appears the same on a small screen device as it does on a larger screen device.
Scan a Barcode to Access a Route or Checkpoint
This topic describes how to access a Route or Checkpoint by scanning its assigned barcode.
Before You Begin
- Assign a Scan ID to the Route or Checkpoint.
- To access a Route for data collection, the Route must be due or overdue.
Procedure
Results
- If the barcode that you scanned is associated with a Checkpoint on the current Route as well as a Checkpoint on a different Route, the Checkpoint on the current Route opens automatically.
- If the barcode that you scanned is associated with a Route that is not the current Route, a window appears that allows you to navigate to the Route that you want to access.
- If the barcode that you scanned is associated with a Checkpoint on more than one Route but not on the current Route, a window appears that allows you to navigate to the matching Checkpoint whose related Checkpoint Task has the earliest Next Date. If multiple Checkpoints have the same Next Date, you can navigate to the first Route, sorted alphabetically, that contains the Checkpoint.
Provide Readings for a Measurement Location
This topic describes how to provide readings for a Measurement Location on a Route.
About This Task
Procedure
Results
- A Reading record is created.
- Readings are saved automatically.Note: The
icon indicates that a reading is successfully saved to the device. - The progress bar that appears in the Route Map pane and in the RDC Overview page in the Overdue Items and Due Items sections is updated to reflect the number of checkpoints for which you have provided readings as well as the percentage of the Route that is complete.
- If the value that you entered in the Reading box is normal, then the Measurement Location is marked with a
icon on the Route Map pane. - If the value that you entered in the Reading box is in alert, then a message appears below the Reading field, specifying the action that you should take. The Measurement Location is marked with a
icon in the Route Map pane.
Provide Readings for a Lubrication Requirement
This topic describes how to provide readings for a Lubrication Requirement on the Route.
Procedure
Results
- A Reading record is created.
- Readings are saved automatically.Note: The
icon indicates that a reading is successfully saved to the device. - The progress bar that appears in the Route Map pane and in the RDC Overview page in the Overdue Items and Due Items sections is updated to reflect the number of checkpoints for which you have provided readings as well as the percentage of the Route that is complete.
- If you selected Skip in the Completion Status box, the Lubrication Requirement record is marked with a
icon in the Route Map pane. - If you selected Done in the Completion Status box, the Lubrication Requirement record is marked with a
icon in the Route Map pane.
Provide Readings for an Asset
This topic describes how to provide readings for Checkpoints in the workspace for a selected asset on a Route.
Procedure
Results
- A Reading record is created.
- Readings are saved automatically.Note: The
icon indicates that a reading is successfully saved to the device. - The progress bar that appears in the Route Map pane and in the RDC Overview page in the Overdue Items and Due Items sections is updated to reflect the number of checkpoints for which you have provided readings as well as the percentage of the Route that is complete.
Create a Recommendation in the Workspace for a Checkpoint
Before You Begin
About This Task
- New Recommendation: This Rounds recommendation is linked to the checkpoint.
- Standalone Recommendation: This Rounds recommendation is linked to the asset that is associated with the checkpoint.
Procedure
Results
- The recommendation that you have created is listed in:
- The Recommendations section on the RDC Overview page.
- The Recommendations pane of the Route, both in the Rounds Designer module and the Rounds Data Collection module.
- If you attached an image to the recommendation, a Reference Document record for the image is linked to the recommendation and to the related checkpoint.
Create a Recommendation in the Workspace for an Asset
Before You Begin
About This Task
- New Recommendation: This Rounds recommendation is linked to the checkpoint.
- Standalone Recommendation: This Rounds recommendation is linked to the asset that is associated with the checkpoint.
Procedure
Results
- The recommendation that you have created is listed in:
- The Recommendations section on the RDC Overview page.
- The Recommendations pane of the Route, both in the Rounds Designer module and the Rounds Data Collection module.
- If you attached an image to the recommendation, a Reference Document record for the image is linked to the recommendation and to the related checkpoint.
Mark a Route Done
About This Task
Procedure
- Mark a Route done from the Route Map pane.
- Mark a Route done from the Due Items or Overdue Items section.
- Mark a Route done from Assigned Routes section.
Results
- If you are working online, the Route no longer appears in the Due Items or Overdue Items section on the RDC Overview page.
If you are working offline, the Route continues to appear in the Due Items or Overdue Items list, as applicable, with information about the Route completion.
Tip: If you are offline, you can select Edit Comment to modify the comment that you entered when you marked the Route done. - A Route History record is created and displayed in the Route History section of the Route when you access it via the Rounds Designer module.
.
.
.