You do not have the latest version of Operations Hub! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Operations Hub product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Access the Trend Chart with Asset Model
Procedure
Create a data source to connect to the Historian server. For instructions, refer to the Data Sources section of the User Guide.
Set up the Historian server. For instructions, refer to the Administration section of the User Guide.
Import the model to Operations Hub. For instructions, refer to the Administration section of the User Guide.
For the model that you have imported, enable the trendable properties by performing the following properties:
In the Admin workspace, select Visualizations > Designer.
For each data variable that is trendable, select the check box in the Trendable check box.
Access the Historian Analysis application. For instructions, refer to the Applications section of the User Guide.
Results
When you navigate to the model, the trend chart plots data based on the selected context.