You do not have the latest version of Operations Hub! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Operations Hub product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Import a Certificate
About this task
Using the Certificate Management tool, you can import the following types of certificates:
Server certificates: You can import a certificate (chain) file of the PEM, PFX, or P12 format. To import a certificate of the PFX or a P12 format, you must enter a password.
Issuer certificates: You can import a certificate file of the PEM format that contains only one certificate for the root CA. If you are currently using a certificate for the external UAA instance, it is replaced by the imported certificate.
Procedure
Double-click .
Tip: By default, this icon appears on the desktop after you install Operations Hub.
The GE Operations Hub Certificate Management Tool page appears, displaying the Server Certificate section.
If you want to import a server certificate, perform the following steps:
In the Imported Certificate subsection, next to the Certificate File box, select Select.
Navigate to and select the certificate file, and then select Open.
Next to the Key File box, select Select.
Navigate to and select the key file, and then select Open.
If you have selected a PFX or a P12 file, enter the password in the Password box.
Select Import.
A message appears, asking you to confirm that you want to import a certificate.
Select Yes.
The certificate is imported.
If you want to import an issuer certificate, perform the following steps:
In the External Trust subsection, next to the Certificate File box, select Select.
Navigate to and select the certificate file, and then select Open.
Select Import.
A message appears, asking you to confirm that you want to import a certificate.
Select Yes.
The certificate is imported and replaces the currently used certificate for the external UAA, if any.