Before you begin
Only a single user can log in to
Operations Hub at a time. Therefore, if you want to log in as a different user, you must first log out of all the
Operations Hub sessions (including the Site Admin console and applications created using
Operations Hub).
Procedure
- In a web browser, enter the
server name
. Alternatively, you can use the shortcut provided on the desktop after installation. - Log in with the credentials you specified when you created a tenant.
- Log in with the credentials that you specified during installation.
Results
The Operations Hub home page appears.
What to do next
Depending on the Operations Hub solution you purchased, perform one of the following steps:- If you have installed Operations Hub by downloading it from Salesforce, run the convertor tool to access the Site Admin console, which is used to configure an MQTT server or an email server.
Note:
- Log out and close all the browser windows before you run the convertor tool.
- Make a note of the credentials of the Site Admin console. If, however, you have not made a note of the credentials when running the convertor tool, reinstall the tool and note down the credentials.
- Even if you change the password of the Site Admin console a second time, when you run the convertor tool, the login page contains the old password. Therefore, you must replace the value in the password field with the new one.
- The Site Admin console if used to configure MQTT settings or an email server. Do not use the Site Admin console to change the password.
- If you have configured Historian UAA as the external UAA to be used with Operations Hub, you can change the password only after performing the following steps:
- Access the uaa.yml file. By default, this file is located in the following folder: C:\Program Files\GE Digital\UAA
- Add the following line at the end of the uaa.yml file:
issuer: uri: https://historian:8443/uaa
. Do not enter a leading space before the line. - Restart the Historian Embedded Tomcat Container service.
- If you have installed the Operations Hub add-on for Historian, access the Historian analysis application. This is the only application you can access. You cannot modify or delete this application.