Map Existing UAA Groups With Operations Hub UAA
About this task
If you want users from an existing instance of UAA to use Operations Hub, you must map the corresponding UAA groups with an Operations Hub UAA group, which is created during Operations Hub installation.
Procedure
- Double-click
.
Tip: By default, this icon appears on the desktop after you install Operations Hub.The UAA/LDAP Connectivity Tool page appears. - Select the Map Existing UAA Groups check box.
- In the UAA Connection section, provide values as specified in the following table.Important: The values that you provide in this step must match the values that you provided in the User Authentication and Authorization Service page while installing Operations Hub. These values are required to connect to the Operations Hub UAA. Operations Hub works only with a single instance of UAA, which is specified during Operations Hub installation. After installation, you cannot change the instance of UAA that Operations Hub will use.
Box Description URL Enter the authorization server URL of the Operations Hub UAA that you specified in the UAA Base URL box during installation (for example, https://localhost). If referencing Historian 7.x UAA, then use a url of https://Historian7x:8443; if referencing Historian 8.x then use a URL of https://Historian8x (no port number). The port numbers reflect the default port numbers for Historian. If ports were customized, then use the selected port.
Client ID Enter the client ID of the Operations Hub UAA server that you specified in the Admin Client ID box during installation. Client Secret Enter the client secret configured for the OAuth client that you specified in the Admin Client Secret box during installation. - Select Test.If connection to the UAA server is established, a message appears, confirming the same.
- Select Continue.In the UAA Mapping section, the drop-down list box contains a list of groups in Operations Hub UAA. In the Filter box, a list of groups in the existing UAA instance appear.
- In the drop-down list box, select the Operations Hub UAA group to which you want to map the existing UAA groups.
- In the Filter box, select the check boxes corresponding to the existing UAA groups that you want to map. Note: If a group is already mapped to the Operations Hub UAA group that you have selected, the check box is already selected.
- Select Map Members.A message appears, confirming that the Operations Hub UAA group is mapped to the existing UAA groups that you have selected.
- Repeat steps 6 through 8 for all the Operations Hub UAA groups that you want to map.