Overview Statistics by Path Web Part

The Overview Statistics by Path Web Part displays important key performance indicators for a production execution path over a specified period of time. The following key performance indicators are displayed:

  • Production: The actual production and target production are displayed for the specified production execution path over the specified period of time. Click the icon to view the Production Distribution Charts By Units Web Part.

  • Waste (%): The actual waste percent and the target waste percent are displayed for the specified production execution path over the specified period of time. The actual waste percent is calculated by Waste / Production. Click the to view the Waste Distribution Charts By Units Web Part.

  • Downtime (%): The actual downtime percent and target downtime percent are displayed for the specified production execution path over the specified period of time. The actual downtime percent is calculated by Downtime / Production. Click the icon to view the Downtime Distribution By Units Web Part.

  • Efficiency (%): The actual efficiency percent and target efficiency percent are displayed for the specified production execution path over the specified period of time.

  • Current Order: The current process order for the selected execution path. Click the to view a list of process orders.

  • Next Order: The next process order for the selected execution path.

  • Sched. Deviation: The amount of time the actual end time deviated from the forecast end time.

  • Inventory: The amount of inventory on the specified production execution path over the specified period of time. Click the to view the Inventory Distribution Charts By Units Web Part.

The reporting time period is displayed at the bottom of the Web Part. To adjust the reporting period, click the Clock icon.

To use this Web Part, you must first:

  • Configure your plant model. For more information on this topic, click here.

  • Calculate the production metric. For more information on this topic, click here.

  • Track waste. For more information on this topic, click here.

  • Track downtime. For more information on this topic, click here.

  • Configure the efficiency metric. For more information on this topic, click here.

  • Configure a production execution path. For more information on this topic, click here.

  • Track inventory. For more information on this topic, click here.

Overview Statistics By Path Web Part

To configure the Overview Statistics by Path Web Part

  1. Create the web part. How?

  2. On the Report Parameters tab, click the Edit Parameter button.

  3. On the Path tab, select the production execution path.

  4. On the Finish tab, click Finish.

See Also