Deploy the Automatic Data Loader Job
Set up the Automatic Data Loader Job
Before You Begin
APM Connect must be installed.
Procedure
Results
The job conductor indicates that the job ran successfully, and the automatic data loader directories will be created if they do not already exist.
You can now place workbooks in the appropriate data loader directory.
Configure the Context File
Before You Begin
The context file provides the automatic data loader job with the information it needs to locate the directories and log the file it requires.
You should have imported the automatic data loader job.
Procedure
Use the Automatic Data Loader
Use the Automatic Data Loader job to manually or programmatically load asset data to APM.
About This Task
By default, the Automatic Data Loader job processes the files in the directories based on the alphanumeric directory name and then the time stamp of the files from oldest to most recent.
Procedure
- Identify the directory that corresponds to the data loader you are using.
- Move the data loader files (either a correctly formatted .xlsx or a .zip file that contains correctly formatted .csv files) into the identified directory.