Overview of Microsoft Azure Support for Proficy Products
Proficy products can be installed on-premises on your local network and within a Microsoft® Azure cloud environment. Proficy products can also communicate across both on premises and cloud environments.
For example, products such as the latest versions of CIMPLICITY, iFIX, Operations Hub, Webspace, OPC UA Server, and Historian can be installed and configured on both local on-premise computers and in Azure cloud images simultaneously, and work together as if they are installed on the same network.
Important: 
    Be aware that knowledge of the Microsoft Azure
      environment is the necessary to configure your system. Azure support is not part of GE Vernova 
      services. You will need to work with your IT department regarding network configuration. This
      guide provides guidelines for doing so.
Note: 
  Be sure to review the hardware and software system requirements for
      the Proficy products you want to use with Azure before implementing your Azure cloud
      environment. It is important that your implementation uses the appropriate product
      recommendations.