Associate Item Example
About this task

Parameters
This function block has the following parameters:
First Blocks Parameters
Parameter | Description |
Source Region ID | SRC1 |
Source Region Location | 1 |
Destination Region ID | DST1 |
Destination Region Location | PRT_LAST |
Item Type | |
Item Class | VEHICLE |
Insert | Insert |
Auto Associate | False |
Second Blocks Parameters
Parameter | Description |
Source Region ID | SRC2 |
Source Region Location | 1 |
Destination Region ID | DST1 |
Destination Region Location | PRT_LAST |
Item Type | |
Item Class | VEHICLE |
Insert | Add |
Auto Associate | False |
Procedure
- An Output Module with two Associate Item Blocks is executed.
- The first block takes the item from the head location of Region SRC1 and inserts it into the tail location of region DST1.
- The second block takes the item from the head location of region SRC2 and adds it to the tail location of region DST1.