Object Form

CimEdit provides you with several tools to adjust an object's form.

The tools include several ways to change its:

  • Size.
  • Shape.
  • Display angle.

Note:
The default unit of measure for screens and objects is points (pt). A point is a printer's basic unit of type measurement. There are 72 points in one inch.

There are many places in CimEdit where you are asked to enter location, size, or units as a number and a unit of measure. In addition to points, you can use any of the following for a unit of measure in CimEdit:

" Inches
in Inches
mm Millimeters
cm Centimeters
twips 1/20th of a point

If you enter any of these other units of measure, the measurement will be automatically converted to points by CimEdit.

For example, if you enter horizontal and vertical grid units of .5" in the Options dialog box for Tools, when you apply the change, the values will be displayed as 36 pts.