User Configuration

Review existing users

Procedure

  1. To review exiting users, expand the Security folder in the left pane of the Workbench.
  2. Select Users.
    The Workbench right pane can display the following attributes for each User.
    AttributesDescription
    User ID A name that uniquely identifies each user.
    Enable Indicates if the account is enabled or disabled.
    Password Needed If a password is needed for the selected user.
    Windows User Identifies users who are authorized by Windows authentication.
    Role ID The role assigned to the user. This determines the privileges assigned to the user.
    User Name The user's name.
    Note:
    Use the Workbench Field Chooser to remove or re-display any of the fields, except the User ID. The User ID is required.

    The User list is initially sorted by User ID. You can click any of the other column titles at the top of the list to sort the list by that attribute.