Create Charts to Visualize Time Series Data
About Creating Visualizations for Time Series Data
Advanced Visualization enables you to create visualizations for the time series data that is collected for the asset tags over a specified time period. For more information on retrieving the time series data for asset tags, refer to the Time Series Data Retrieval Service topic in the Time Series Data help.
You can use the tag browser to access the assets available for your tenant and select the associated asset tags for which you want to retrieve the time series data. Advanced Visualization provides a curated data source for visualizing time series data. The data source is designed using a reporting object and contains fields that can be used to create time series data charts. Based on the selected asset tags and the fields selected from the data source, you can create and customize the visualizations for time series data.
Additionally, using the charts created for time series data, you can create a dashboard. The dashboard has filtering capabilities that allow you to either specify filter criteria to view data for a predefined period of time, or configure a custom date range to display data that matches the duration.
About the Tag Browser
The Tag Browser enables you to choose assets and the associated asset tags to visualize the time series data retrieved for the tags.
- Asset Browser: Enables you to select the assets associated with the asset tags for which you want to visualize the time series data. When you select an asset, the asset and the associated assets tags appear in the Tag Browser section.
- Tag Browser: Enables you to select the asset tags for which you want to visualize the time series data. When you select an asset tag, it appears in the Plotted Tags section. Based on the plotted tags and the fields selected from the Time Series Data data source, the visualizations displaying the time series data are created.
- Settings: Contains the following settings:
- Time Span: Enables you to specify the time period for which you want to visualize data when the visualization is created. When you run the visualization, the data for the specified time period appears by default.Note: The default time period selected in the Time Span drop-down list box is one week.
- Data Operation: Enables you to configure the type of data that you want to visualize. Based on your selection, the raw or interpolated time series data appear on the visualization. For more information on the raw and interpolated data types, refer to the Time Series Data help.
- Time Span: Enables you to specify the time period for which you want to visualize data when the visualization is created. When you run the visualization, the data for the specified time period appears by default.
Create a Chart or Dashboard to Visualize Time Series Data
Procedure
Switch Assets in a Time Series Dashboard
Before You Begin
- The asset to which you want to switch must be of the same type as the current asset (for example, pumps, compressors, turbines).
- Time Series data for both the assets must already be plotted.