Permission Sets
About Permission Sets
Permission sets specify the actions users can take and the assets on which they can act.
To control user access to APM, as a user administrator, you assign permission sets (actions) and one or more assets to individual users or user groups.
Keep the following in mind when planning for permission sets and user access:
- You can define multiple permission sets. Each permission set can have one or more features.
- You can assign one or more permission sets to a single user. For example, you can do this when you first add the user to APM.
- You can assign one permission set per user group. User groups provide a convenient and powerful way to manage access for multiple users.
- You can assign a user to multiple user groups. When you add a user to a user group, the user receives its associated permission sets as defined in the user group definition.
Default Permission Sets
The default permission sets are specified in the table.
You can view the following default permission sets on the Permission Sets page.
Tip: Select the permission set to view all available permissions (actions) for the permission set.
This Permission Set: | Can do this: |
---|---|
APM Next | Allows you to access APM. Important: Ensure that the APM Next permission set is activated for all the users. Only then, users can access APM. If you have upgraded from a previous version, the GE Vernova Customer Support team automatically activates the APM Next permission set for all the existing users. For new users, however, you must activate the permission set. |
Foundation Admin | Has administrator permissions for the Cloud APM application. |
APM Basic User | Access Applications menu, tools, and basic applications. Note: If present, this permission set should be selected for all users in the tenant. |
User Admin |
|
Ingestor Admin | Users with the Ingestor Admin role have privileges for the ingestion process. |
M&D Manager | May be assigned permissions to specific MicroApps, such as Alerts, Cases, Analysis, Asset, or Analytics. |
SmartSignal | Has administrator permissions for SmartSignal. |
AnalyticsExecutorRole | Has permissions for the following permission sets:
|
Custom |
|