Analysis Charts
About Analysis Charts
Analysis charts appear on cards contained in a view.
Up to eight charts can exist on a card.
Charts appear on an Alert Analysis or Analysis View and can be modified and saved as an Analysis Template. You can select or co-render multiple groups containing multiple charts.
When a chart is saved as a template and added to an Alert Template, any triggered alerts appear in the Alerts module, where they can be examined.
Analysis allows you to access private or public templates, or a new Time Series Analysis or Event Data Analysis view in the View Selector after you have chosen an asset context.
Analysis allows you to access data of assets that are not available in APM. You can upload a CSV or XLXS file containing data of assets using the New CSV Template. This data is used to create the appropriate tags in the Analysis Tag Browser. Using these tags you can plot charts to perform the CSV analysis.
If you update or save a new template, the Context Ribbon appears, where you can change the template name, designate the template as public or private, and determine if the template is for an instance or a class.
The selected configuration or the default value for the Time Zone (), Data Resolution (
), Data Source (
), System of Measure (
), and Data Quality (
) drop-down list boxes appears for each settings option. You can select different options in these list boxes. These options are not available for SmartSignal charts.
The default date range for an Alert Analysis has a start date seven days before the event date and an end date seven days after the event date. If the current date is earlier than the computed end date (seven days after event date), the end date defaults to the current date.
The default date range for a Time Series Analysis View has a start date of 15 days before the current date.
The Event Data Analysis View uses a selected number of events prior to a date and time selected by you to determine the time range for the selected event type. You can also select the number of seconds pre- and post-events to refine the amount of data surrounding the selected events.
As you plot tags for an Alert Analysis View or a Time Series Analysis View, a Plotted Tags list appears in the Tag Tree Browser. The list appears as a hierarchy with nodes for cards and charts, and plotted tags or plotted tag series listed below.
Event Data Analysis view chart types are limited to X-Y or Polar charts. After you have selected the number of events for an Event Data Analysis view, added two tags, and selected View Data, an Event Frames list appears in the Tag Tree Browser that contains the number of events selected. Each event is identified by a date and time and is global for the all charts on the view. As you add cards and plot tags, a Plotted Tags list appears. Tags are represented below the main card node. You cannot manipulate tags in the Plotted Tags list. Muting and unmuting of data is controlled in the listed event frames, not the plotted tags. The Event Data Analysis View does not support multiple assets.
- Sort by muted tags.
- Sort by tag name.
- Sort by value.
- Use the left or right arrow to page through multiple pages.
- Show combined data. Select the arrow down or up to view in ascending or descending order.
- Show muted data.

- Show tag information.
- Add a chart below the selected chart.
- Modify a chart.
- Arrange a chart.
You can select to delete a chart.
Adding a new chart to a card creates an empty chart below the selected chart.
- Selection of common chart controls such as zoom, cross-hair, and so on is applied across all the charts in a card and also across all the charts in any other card in the view. Any new charts added to the cards also retain the common chart controls selection made in one card. Deleting the chart or the card or moving to another card does not change the common chart controls selection. The sub configuration options of the common chart controls do not open for all the charts on which the selection is propagated.
- The common chart control selections are reset when you select another chart control outside the common controls and refresh the chart.
- When navigating to Analysis from an Alert, the selection of common chart controls is retained on the charts.
- The selection of common chart controls is retained on the Event Data Analysis charts.
Create a Time Series Analysis Chart
Use Time Series Analysis to review data requests, or to create new analysis view templates.
About This Task
You can select the type of ad hoc analysis charts with which you want to work. The Time Series Analysis uses time series data for the asset context you select. You can save a Time Series Analysis view as a template, which can then be applied to an Alert Template, triggering an alert in the Alert module.
You can add additional assets, add cards and charts, select a layout, change the date range, mute and unmute tags, plot tags, filter tags, plot tag expressions, and make other necessary modifications.
Procedure
Create an Event Data Analysis Chart
Use Event Data Analysis to review event data, or create new analysis view templates.
About This Task
Event Data Analysis allows you to compare the same event occurrence over time to see if it indicates a gradual degradation of an asset.
You can save an Event Data Analysis view as a template, which can then be applied to an Alert Template, triggering an alert in the Alerts module.
The Event Data Analysis charts rely on the selection of an Event Type. Event Types are garnered from Alert Types, which are created for Alert Templates during tenant on-boarding.
Just as with Time Series Analysis charts, you can add cards and charts, select a layout, mute and unmute events, plot tags, filter tags, plot tag expressions, and make other necessary modifications. Event Data Analysis charts are event-frame-centric instead of tag-centric. Event Frames are the timestamped, prior instances of the selected Event Type.
You can select the number of events in the charts, determine the number of seconds prior to and after each event, and determine the date and time ending the event search to appear. The default ending time is the present date and time.
If you change any of the settings for the charts, you must select Update to make the changes in the charts.
- You cannot add multiple assets in the Tag Tree Browser, Tag Expressions or Search Browser panes.
- There is no Chart Register.
- There is no Timeline Slider below the chart.
- There is no Tag Information Table below the chart.
- You are limited to 40 events per tag.
Procedure
Modify a Chart Name
You can change a chart name to better suit the information on a card.
About This Task
When a chart is created, it is automatically named Chart <#>, where (#) is an assigned, incremental numerical value. You cannot remove a chart's name.
Procedure
Add a Cross-Hair to a Chart
About This Task
You can point on a data point in a chart and have that same time reflected as a cross hair across all the charts in the template. It provides the ability for values of the tags appear at mouse point in multiple charts.
The cross hairs applies across all chart types across all cards.
Procedure
Delete a Chart
You can delete a time-series chart in the Ad hoc Analysis instance when two or more charts are present on the card.
About This Task
If you delete a chart, all tags, reference curves and tag expressions unique to the deleted chart are removed from the plotted tags list. If all charts are deleted from a card, you will be able to select a chart type.
Procedure
Resize an Analysis Chart
About This Task
Procedure
Change the Tag Color or Style
About This Task
Procedure
- In the Applications menu, navigate to the HEALTH section, and then select Analysis.
- Use the Context Browser to select an asset context.
- In the View Selector, select a Public Templates or My Templates view.
- In a view with at least one chart with plotted tags, select the drop-down arrow from the Plotted Tags for the Tag Style options to appear for all the charts on the view.
- From the Tag Color section, select the color you want to use.
- From the Line Style section, select the check box next to the line you want to use.
- From the Point Shape section, select the check box next to the shape you want to use.
- Select Submit. If you do not want to change the current settings, you can select Cancel to return to the previous screen without any changes.
Display Tag Information
You can view information about plotted and unplotted tags in various ways.
About This Task
You can view a template and where the tags are plotted on the charts. You can hover over the plotted tags to view additional information about tags, tag name, and asset name that appears in the tree.
You can view information about an unplotted tag in the Tag Tree Browser, and you can view information about a plotted tag in the Plotted Tags section on the Tag Tree Browser, and on an Alert Analysis chart or an analysis chart. There are several ways to view information about a tag:
You can view information about an unplotted tag in the Tag Tree Browser, and you can view information about a plotted tag on an Alert Analysis chart or an Analysis chart.
There are several ways to view information about a tag:
Doing this | Allows you to view this |
---|---|
Hover over the data on a chart. |
For all tags listed in the chart Register:
Note: Changing the time zone affects how the timestamp is displayed.
|
Hover over tags in the chart Register. | Each tag plotted in the chart has an entry in the Tag Register. When you hover over the name of a tag in the register, the following details appear:
|
Hover over tags in the Plotted Tags section of the Tag Tree Browser. |
For a selected sensor generated tag on the Tag Tree Browser:
|
Hover over an unplotted sensor generated tag in the Tag Tree Browser. |
For a selected sensor generated tag on the Tag Tree Browser:
|
Hover over an unplotted asset attribute in the Tag Tree Browser. | For a selected asset attribute on the Tag Tree Browser:
|
Hover over an unplotted tag expression in the Tag Tree Browser. | For a selected tag expression on the Tag Tree Browser:
|
Use the Chart Option to view a table of plotted tag information on a chart. |
For all tags listed in the chart Register:
|
Procedure
Mute Tags on a Chart
About This Task
- This feature is applicable only to the following views:
- Ad hoc and saved template views for Time Series Analysis.
- Ad hoc view for CSV Analysis.
- This feature is not applicable to SmarSignal cards.
Procedure
Access Data Delta
About This Task
You can view the time stamps and the difference in time between the two points selected on the Time Series charts. You can also view the delta between the values of the tags for the selected time stamps.
Procedure
Pan the Chart Data
Use panning to display data earlier or later than the date range displayed on the chart.
About This Task
You can pan chart data for both a Time Series Analysis and an Event Data Analysis view.
Procedure
- To pan an Alert Analysis chart:
- To pan an Analysis chart:
- To reset the pan to the date range selected, in an alert analysis chart or an analysis chart, select
, and then select
to hide the reset panel.
Reorder Axes on a Chart
When you drag tags into a Parallel Axis chart, the order in which you plotted the tags matches the displayed order of the axes on the chart.
About This Task
You can change the order of the Y-axes after you have plotted at least three tags.
Procedure
Emphasize Data on Vertical Axes for a Chart
To manage tags, you can emphasize data on multiple chart axes, and select multiple areas on one axis to emphasize.
About This Task
You can de-emphasize extraneous data for Y-axes, displaying the irrelevant data as faded lines. You also can resize the selector boxes added to an axis.
Procedure
- To select a data portion to emphasize:
- To enlarge or reduce the area, select one end of the selector box and drag to make the area larger or smaller.
Change Chart Direction
Polar charts are directional (clockwise or counter-clockwise).
Procedure
Access Data Points on Charts
About This Task
Procedure
- To access data points on an analysis chart:
- To clear all access data points on an analysis chart:
Filter Data Points on Charts
About This Task
You can filter selected data points in a chart and have the same time reflected across all charts in a template. You can filter data such that the selected data is visible in all the charts or excluded in the charts. This helps you to focus on the relevant data based on the selected data points and filter options in lasso selection. You can also use the lasso selection on a chart to filter out data in combination with other filters such as condition and value based filters, zoom options, and mute tags options. This feature is available for Time Series charts, Parallel Axis, X-Y charts, Spiderweb, and Bar charts. You can enable this functionalty only in the Time Series Analysis and the CSV Analysis views.
Procedure
Upload a CSV file
You can upload a CSV file with data using the New CSV Template that is available in the Analysis view templates drop-down list.
About This Task
Using the CSV upload feature you can view data of assets that are not available in the APM server and visualize the data using the tags that are created for the uploaded data.

- Tag NameNote:
- The tag name can include special characters.
- Each AssetName can be combined with the TagName, for example G12.DWATT.
- Date and Time
- Data for each tag
- The columns between the tag keywords and tag name must not be empty. All other columns can be empty.
- Some rows can be empty.
- The Tags and description keywords columns must have the timestamps for the tag data in the column that follows the tags.
- The Tag column names must be prefaced with the keyword Tag/Tags.
- The UoM column names must be prefaced with the keyword Unit/Units.
- The tag description column name must be prefaced with the keyword Description.
- The keyword prefixed rows must be prior to the timestamp data rows.
- The file format must be .csv or .xlsx.
- Row with a NaN timestamp is not considered.
- For an empty or a non-numeric data row, the column data for the tag is considered as NaN.