Calibration Assessment
Calibration Management: Calibration Assessment Workflow
This workflow describes the process of performing a calibration, verifying and saving the results, and proposing and approving recommendations via a manual calibration, a Fluke Documenting Process Calibrator, or a GE Druck Calibrator.
In the following workflow diagram, the blue text in a shape indicates that the corresponding description has been provided in the sections that follow the diagram.

View Task
Persona: Technician
The task is the calibration task that a calibration technician is expected to perform. The calibration task describes the asset to be calibrated, the calibration profile to be used, the tools to be used and other pertinent information related to the task.
Manual Calibration?
Persona: Technician
Identify whether you want to perform a manual calibration or an automated calibration.
- In a manual calibration, you print the Calibration Template, note the readings, and then create a Calibration Event manually to store the readings.
- In an automated calibration, you send the templates to a documenting process calibrator, perform the calibration, and then receive the data from the calibrator.
Send for Calibration
Persona: Technician
If you are performing an automated calibration, you must send the Calibration Templates to the documenting process calibrator.
Calibration Planning
Persona: Technician
Go to the Calibration Planning workflow.
Print Calibration Template
Persona: Technician
If you are performing a manual calibration, print the Calibration Template. While performing calibration in the field, you can then enter the readings on the printed template.
Perform Calibration
Persona: Technician
If you are performing a manual calibration, note the readings for each test point on the Calibration Template that you have printed. Then, in APM, create a Calibration record, and then enter the noted readings. If you are performing an automated calibration, verify the readings in the calibrator, and then save them. The calibrator displays the error at each test point.
As Found Calibration Pass?
Persona: Technician
In the Calibration record, determine if the As Found calibration has passed. If it has not, you will have to recalibrate the asset.
As Left Calibration Pass?
Persona: Technician
After recalibrating the asset, enter the readings in the same Calibration record in which you entered the As Found readings. Determine if the As Left calibration has passed. If it has not, you must replace or repair the asset.
Replace or Repair Equipment
Persona: Technician
If the As Left calibration fails, then you must replace or repair the asset before recalibrating it again.
Create Calibration Event
Persona: Technician
Create a Calibration Event to store the readings gathered from the manual calibration, and then enter those readings in the Calibration Event record.
Recalibrate
Persona: Technician
If the calibration fails, you must recalibrate the asset.
Receive from Calibration
Persona: Technician
If you have performed an automated calibration, connect the calibrator to APM, and then receive the data from the calibrator. After you save the data, Calibration records are created for each calibration that you have performed using the calibrator.
Create Recommendation
Persona: Technician
You can create a recommendation to suggest ways to improve the calibration results or to prevent overt failures such as broken electrical conduit, failure of a protective element, rusted wires, or the presence of excess moisture.
Approve Recommendations
Persona: Analyst
Approve recommendations by changing the value in the Status field of the recommendations that you want to approve to Reviewed.
Manage Performance Recommendation
Persona: Technician, Analyst
Manage performance recommendation is a subprocess managed outside of calibration management module.
Go to the Action Management: Manage Recommended Actions Workflow.
Approve and Close Calibration Events
Persona: Analyst
Verify the results of the calibration, and then close the calibration. After you close the calibration, all the other fields in the Calibration are disabled, and the associated Calibration Task is cycled.
Ad-Hoc Calibration
Persona: Analyst
Ad-Hoc calibration is performed on the asset that needs to be calibrated outside of its calibration schedule. A predefined calibration task controls the schedule. Therefore, the Ad-Hoc Calibration check box available to the user allows the user to calibrate an asset without recycling the task associated with that asset.
Calibration Task Cycled
Persona: Analyst
After you close the Calibration Events, the associated Calibration Task is cycled automatically. If the task is recurring, then the Last Date and the Next Date fields are updated. If the task is not recurring, then the task is set to complete, and is removed from the Calibration Queue section.