Create an OPC Classic Data Access (DA) Collector
Before you begin
- Deploy Proficy Historian for AWS.
- Install collectors. You can install them on-premises or on a VPC (which can be different from the one on which Proficy Historian for AWS is deployed).
About this task
The OPC Classic DA collector collects data from any OPC 1.0 or OPC 2.0 compliant OPC server. The collector automatically determines the capability of the OPC server to which it is connected and supports appropriate features based on this information.
Features:
- You can browse the source for tags and their attributes on an OPC server that supports browsing.
- Both the polled and unsolicited data collection are supported; when changes
to the OPC source tags are detected, they are sent to the Historian server.
Unsolicited data collection is supported for OPC 2.0 only. The minimum poll
interval is 100ms. The collector duplicates raw samples from the OPC server
into the Historian data archive.
For unsolicited data collection, if collector compression is disabled, all new values produce an exception. And, the deadband percentage is determined by the collector deadband percent. You can only configure the collector deadband percent by enabling compression.
- The supported timestamp resolution is 1ms.
- Floating point, integer, binary, and string data are supported.
- Python expression tags are supported.
- Device timestamps are accepted.
Supported data types:
The OPC Data Type | Recommended Data Type in Historian |
---|---|
I1 - 16 bit signed integer | Single Integer |
I4 - 32 bit signed integer | Double Integer |
R4 - 32 bit float | Single Float |
R8 - 64 bit double float | Double Float |
UI2 - 16 bit unsigned single integer | Unsigned Single Integer |
UI4 - 32 bit unsigned double integer | Unsigned Double Integer |
UI8 - 64 bit unsigned quad integer | Unsigned Quad Integer |
I8 - 64 bit quad integer | Quad Integer |
BSTR | Variable String |
BOOL | Boolean |
I1 - 8 bit single integer | Byte |
Note: The collector requests data from the OPC server
in the native data type. Then the collector converts the received value to a
Historian Data Type before sending it to the data archiver.
Supported tag attributes:
- Tagname
- Source Address
- Engineering Unit Description
- Data Type
- Hi Engineering Units
- Lo Engineering Units
Procedure
- Run Command Prompt as an administrator.
- Run the CloudHistorianConfigurationUtility.exe file. It is provided along with the collectors installer. After you install collectors, it will be available in the C:\Program Files\GE Digital\Historian Cloud Config folder by default.
- Enter the number corresponding to creating a collector instance.
-
Enter the following details:
Field Description NLB DNS Enter the Amazon Network Load Balancer (NLB) DNS.
Tip: To find the NLB DNS:- Access the EKS cluster on which you have deployed Proficy Historian for AWS.
- Access the EC2 instance.
- In the navigation pane, under Load Balancing, select Load Balancers.
- Select the load balancer for which you want to find the DNS.
- In the Description section, copy the DNS name.
Username Enter the username to connect to Proficy Historian for AWS. Password Enter the password to connect to Proficy Historian for AWS. Tip: This is the value you entered in the Password field under UAA Configuration when you created the stack.A list of collector types appears. - Enter the number corresponding to the collector that you want to create.
-
Enter the following details:
Field Description Interface name Enter a unique interface name for the collector. OPC server Enter the prog ID of the OPC Classic server. The OPC Classic DA collector is created. - Start the collector instance (as a WIndows service).