Create an OPC UA Data Access Collector

Before you begin

  1. Deploy Proficy Historian for AWS.
  2. Install collectors. You can install them on-premises or on a VPC (which can be different from the one on which Proficy Historian for AWS is deployed).

About this task

The OPC UA DA collector collects data from a OPC UA 1.0 and OPC 2.0-compliant OPC UA DA server. The collector automatically determines the capability of the OPC UA DA server to which it is connected, and supports the appropriate features based on this information.
Features:
  • You can browse the source for tags and their attributes on an OPC server that supports browsing.
  • Both the polled and unsolicited data collection are supported; when changes to the OPC source tags are detected, they are sent to the Historian server. Unsolicited data collection is supported for OPC 2.0 only. The minimum poll interval is 100ms. The collector duplicates raw samples from the OPC server into Data Archiver.

    For unsolicited data collection, if collector compression is disabled, all new values produce an exception. And, the deadband percentage is determined by the collector deadband percent. You can only configure the collector deadband percent by enabling compression.

  • The supported timestamp resolution is 1ms.
  • Floating point, integer, binary, and string data are supported.
  • Python expression tags are supported.
  • Device timestamps are accepted.
Supported data types:
OPC UA DA Collector Data Type Recommended Data Type in Historian
OpcUaType_Null ihTKVariableString
OpcUaType_Boolean ihTKBool
OpcUaType_SByte ihTKByte
OpcUaType_Byte ihTKByte
OpcUaType_Int16 ihTKInteger
OpcUaType_UInt16 ihTKUInt16
OpcUaType_Int32 ihTKDoubleInteger
OpcUaType_UInt32 ihTKUInt32
OpcUaType_Int64 ihTKInt64
OpcUaType_UInt64 ihTKUInt64
OpcUaType_Float ihTKFloat
OpcUaType_Double ihTKDoubleFloat
OpcUaType_DateTime ihTKVariableString
OpcUaType_Guid ihTKDataTypeUndefined
OpcUaType_StatusCode ihTKDataTypeUndefined
OpcUaType_String ihTKVariableString
OpcUaType_ByteString ihTKDataTypeUndefined
OpcUaType_XmlElement ihTKDataTypeUndefined
OpcUaType_NodeId ihTKDataTypeUndefined
OpcUaType_ExpandedNodeID ihTKDataTypeUndefined
OpcUaType_DiagnosticInfo ihTKDataTypeUndefined
OpcUaType_QualifiedName ihTKDataTypeUndefined
OpcUaType_LocalizedText ihTKDataTypeUndefined
OpcUaType_ExtensionObject ihTKDataTypeUndefined
OpcUaType_DataValue ihTKDataTypeUndefined
Supported tag attributes:
  • Tagname
  • Source Address
  • Engineering Unit Description
  • Data Type
  • Hi Engineering Units
  • Lo Engineering Units

The Engineering Unit Description, Hi Engineering Units and Lo Engineering Units vary based on the OPC server vendor.

Procedure

  1. Run Command Prompt as an administrator.
  2. Run the CloudHistorianConfigurationUtility.exe file. It is provided along with the collectors installer. After you install collectors, it will be available in the C:\Program Files\GE Digital\Historian Cloud Config folder by default.
  3. Enter the number corresponding to creating a collector instance.
  4. Enter the following details:
    Field Description
    NLB DNS

    Enter the Amazon Network Load Balancer (NLB) DNS.

    Tip: To find the NLB DNS:
    1. Access the EKS cluster on which you have deployed Proficy Historian for AWS.
    2. Access the EC2 instance.
    3. In the navigation pane, under Load Balancing, select Load Balancers.
    4. Select the load balancer for which you want to find the DNS.
    5. In the Description section, copy the DNS name.
    Username Enter the username to connect to Proficy Historian for AWS.
    Password Enter the password to connect to Proficy Historian for AWS.
    Tip: This is the value you entered in the Password field under UAA Configuration when you created the stack.
    A list of collector types appears.
  5. Enter the number corresponding to the collector that you want to create.
  6. Enter the following details:
    Field Description
    Interface name of the collector Enter the name that you want to provide for the collector instance. A value is required and must be unique in the DNS.
    OPC UA Server URI Enter the URI to connect to the OPC server in the following format: opc.tcp://<host name or IP address of the OPC UA server>:<port number>
    The OPC UA DA collector is created and started.