Overview of the OPC Classic DA Collector
The OPC Classic Data Access (DA) collector collects data from any OPC 1.0 or OPC 2.0 compliant OPC server (such as CIMPLICITY). The collector automatically determines the capability of the OPC server to which it is connected and supports appropriate features based on this information.
- You can browse the source for tags and their attributes on an OPC server that supports browsing.
- Both the polled and unsolicited data collection are supported; when changes to
the OPC source tags are detected, they are sent to the Historian server.
Unsolicited data collection is supported for OPC 2.0 only. The minimum poll
interval is 100ms. The collector duplicates raw samples from the OPC server into
the Historian data archive.
For unsolicited data collection, if collector compression is disabled, all new values produce an exception. And, the deadband percentage is determined by the collector deadband percent. You can only configure the collector deadband percent by enabling compression.
- The supported timestamp resolution is 1ms.
- Floating point, integer, binary, and string data are supported.
- Python expression tags are supported.
- Device timestamps are accepted.
The OPC Data Type | Recommended Data Type in Historian |
---|---|
I1 - 16 bit signed integer | Single Integer |
I4 - 32 bit signed integer | Double Integer |
R4 - 32 bit float | Single Float |
R8 - 64 bit double float | Double Float |
UI2 - 16 bit unsigned single integer | Unsigned Single Integer |
UI4 - 32 bit unsigned double integer | Unsigned Double Integer |
UI8 - 64 bit unsigned quad integer | Unsigned Quad Integer |
I8 - 64 bit quad integer | Quad Integer |
BSTR | Variable String |
BOOL | Boolean |
I1 - 8 bit single integer | Byte |
- Tagname
- Source Address
- Engineering Unit Description
- Data Type
- Hi Engineering Units
- Lo Engineering Units
- Is Array Tag