Manage Case Templates

Create, Modify, or Delete a Case Template

You can use case templates to add reusable information about a case to a new or existing case.

Before You Begin

When creating a new case template, make sure that the case template does not already exist by searching or scrolling through the available templates in the case templates list. If you attempt to create a new case template with the same name as an existing case template, the following error message will appear: "A case template with that name already exists. Please choose a different name."

About This Task

You can modify an existing case template, or create a new one. The case templates list displays all sections included with the selected template.

Procedure

  • To create a case template:
    1. In the Applications menu, navigate to the HEALTH section, and then select Case Templates.
      Case Templates opens in a new tab.
    2. Select the Add icon ().
      The Case Templates page appears in edit mode.
    3. Use the case template options to add template details in the Interpretation section.
      For this optionDo this
      Case Template Name fieldEnter a unique Template Name.
      Category drop-downSelect the issue from the list.
      Likelihood drop-downSelect how likely the issue is to occur.
      Urgency drop-downSelect how quickly the issue needs to be resolved.
      Symptoms fieldEnter the symptoms that caused the alert for the case into the Symptoms field.
      Diagnosis fieldEnter the apparent cause of the alert and any supporting information into the Diagnosis field.
      Recommendation fieldEnter the recommended actions to take and any supporting information into the Recommendation field.
    4. Select Configure Sections to add a custom section. See the topic "Configuring a Case Template" for more information.
    5. Select Save.
      The new template is added to the Case Template list.
  • To modify the attributes of an existing case template:
    1. In the Applications menu, navigate to the HEALTH section, and then select Case Templates.
      Case Templates opens in a new tab.
    2. In the Case Template list, select the Search icon () to expose the Search field. Enter at least three characters and select Enter to narrow the list.
      To return to the full case template list, select the X next to the Search field.
    3. Select the specified template name.
      The Case Template Edit page appears.
    4. Modify the template details, and then select Save.
      The changed values in the template are saved.
  • To delete a selected case template:
    1. In the Applications menu, navigate to the HEALTH section, and then select Case Templates.
      Case Templates opens in a new tab.
    2. In the Case Templates page, select an existing case template.
      The Case Template Edit page appears.
    3. Select Delete Template.
      Note:

      Deleting a case template does not affect cases where the case template was previously used.

      In addition, if the selected case template is associated with an alert template, a message appears, notifying you that the template cannot be deleted as it is associated with one or more alert templates.

Configure a Case Template

You can configure an existing case template or configure a newly created one.

Before You Begin

You must have permissions to access and modify templates.

About This Task

You can create a new case template and then configure the sections, or configure an existing case template. The following sections are locked and are automatically added to the new template. In addition, they are designated with a padlock icon in the Configure Sections dialog box:

  • Interpretation
  • Closure
  • Analysis
  • Actions
  • Evidence
  • Similar Cases
  • Notes
  • Recommendations
  • Work History
Note: Recommendations and Work History are not available in Legacy Predix Essentials.

Procedure

  1. In the Applications menu, navigate to the HEALTH section, and then select Case Templates.
    The Case Templates page opens in a new tab.
  2. In the Case Templates screen, do one of the following:
    • Select an existing Case Template from the list.
    • Select the Add icon () in the upper-right corner of the page.
    The template appears. For new templates, only the Interpretation section is displayed.
    Note: If this is a new template, you must enter a name for the template in the name field at the top of the screen. Once you have done this, the Save button is activated.
  3. Select Configure Sections.
    The Configure Sections dialog box appears.
  4. Select the section or sections that you want to add.
    Each added section is given a check mark.
  5. Select Apply.
    The dialog box closes and the newly added sections appear in the template.
  6. Select Save to save the changes.
  7. Optional: To remove a section, do the following:
    1. Select Configure Sections.
    2. Select the checked section you want to remove.
    3. Select Apply.
    4. Select Save.
      Your changes are saved.

Sort and Filter Columns in the Case Template Grid

You can sort and filter the list of templates using a column to retrieve the specific required template matching the sorting order and filtering criteria.

Before You Begin

You must have permissions to access and modify templates.

Procedure

  • To sort a column in the Case Templates grid view:
    1. In the Applications menu, navigate to the HEALTH section, and then select Case Templates.
    2. Select a column header, such as Severity.
      The data in the column is sorted either in the ascending or descending order, respectively. To reverse the order, select the column header again.
      Note:
      • Columns are sorted alphanumerically, first by symbols, then number, and then uppercase and lowercase letter.
      • The columns remain sorted in the same order even when you access the details page of a case template, and then navigate back to the Case Templates grid.
  • To filter a column in the Case Templates grid view:
    1. In the Filter text box below the column header, enter the term with which the column is filtered.
      Note: As soon as you type three characters, the column begins to filter the entries. As you continue to type the characters, the column continues to filter the entries, narrowing down the results.
      To find all entries with the Closed Status, enter Clo in the Filter text box for the Status column, and then press Enter.
      The column is filtered, showing all entries with status Closed.
      Note:
      • The filters applied to the columns in the Case Templates grid are persistent even when you access the details page of a case template, and then navigate back to the Case Templates grid.
      • Sorting of a column is not affected by the filtering criteria. For example, if you sort the grid by the Name column, and then filter by Name and ID, the sort order will remain the same.

Show or Hide Columns in Case Templates

You can show or hide one or more columns in a Case Template.

Before You Begin

You must have permissions to access and modify the templates.

Procedure

  • To show a column in the Case Templates grid view:
    1. In the Applications menu, navigate to the HEALTH section, and then select Case Templates.
    2. Select Hide/Show Columns, and then select the check box for each column names that you want the grid to display.
      The selected columns appear in the grid. By default, all column names are selected.
  • To hide a column in a Case Template, select Hide/Show Columns, and then clear the check box for each column name that you want the grid to hide.
    The selected columns do not appear in the grid.

Apply a Case Template to a Case

You can select and apply a case template to a specific case.

About This Task

Case templates contain values that can be applied to a case. You can apply multiple templates to a case. Any applicable values are overwritten by the last template applied.

Procedure

  1. In the Applications menu, navigate to the HEALTH section, and then select Case Templates.
  2. Select a case from the list.
  3. In the Case Details page, select the List icon (), and select Apply Template.
  4. In the Select a Case Template dialog box, enter at least three characters into the Search field.
    The list of case templates narrows as you enter text.
  5. Select a template from the list.
    A message appears indicating that certain sections are overwritten by this action.
  6. Select Apply.
    The content contained in the template is applied to the case.
    Note: You can modify the content values after applying a template.