General Reference

Reference Documents System Requirements

License Requirements

This feature is available with the core Essentials application; no specific license is required.

Record Manager URLs

There are two URL routes associated with Record Manager: record-manager, which opens a record in Record Manager in a new tab, and BDF-screen, which opens a collection of records in the Bulk Data Form in a new tab. There is also an action route, datasheet-dialog, which opens a record in a separate window.
Note: An action route is preceded by ! instead of # when specifying the route in Essentials.

The following table describes the various paths that build on the routes, and the values that you can specify for each element in the path.

ElementDescriptionAccepted Value(s)Notes
#record-manager/<FamilyKey or ID>/<EntityKey>: Opens the Record Manager page for a specified record using the family key or ID.

#record-manager/<FamilyKey or ID>: Opens the Record Manager page for a new record using the family key or ID

#record-manager/<FamilyKey or ID>/<EntityKey>?datasheetid=<DatasheetID>: Opens the Record Manager page for the entity of a given family using the desired datasheet.

#record-manager/<FamilyKey or ID>?<FieldID1>=Value1&<FieldID2>=Value2: Opens the Record Manager page for a new record and updates the specified field with given value.

#record-manager/<FamilyKey or ID>/<Entitykey>?<FieldID1>=<Value1>&<FieldID2>=<Value2>: Opens the Record Manager page for the entity of a given family and updates the specified fields with the given values.

#record-manager/<Family Key or ID>/<EntityKey>?datasheetid=<DatasheetID>&<FieldID1>=Value1&<FieldID2>=Value2: Opens the Record Manager page for the entity of a given family using the desired datasheet and updates the specified fields with the given values.

#record-manager/<Family Key or ID>/<EntityKey>/id/<DatasheetID>?<FieldID1>=Value1&<FieldID2>=Value2: Opens the Record Manager page for the entity of a given family on the desired datasheet and updates the specified fields with the given values.

Family Key Specifies the Family Key of the record that you want to open in the Record Manager. Any Family Key that corresponds to a family. NA
Family ID Specifies the family ID of the record that you want to open in the Record Manager.Alphanumeric Family IDThe Family ID parameter provides the same functionality as the Family Key parameter. In each URL that contains the Entity Key parameter, you can use either the Family Key or Family ID parameter. You do not need to use both.
Entity KeySpecifies the Entity Key of the record that you want to open in the Record Manager.Any Entity Key that corresponds to an existing record in the specified family.

N/A

Datasheet ID Specifies the datasheet that you want to display in the Record Manager.The Datasheet ID of the desired datasheet.The Datasheet ID must correspond to a datasheet that has been defined for the specified family in the Configuration Manager. If you do not specify this parameter, the Essentials system will use the datasheet that the current user was last using when viewing a record in the specified family or the default datasheet if the user has never opened a record in that family before.
Field ID Defines fields that you want to populate automatically, as well as the values that you want to use to populate them.Values that are appropriate for the specified fields.You can specify values that will be used to populate fields in that record automatically. The actual parameter names should correspond to fields that you want to populate. You must use the Field ID as the parameter name. The parameter values will vary depending on the values that you want to use to populate the fields, but you should make sure to specify values that are appropriate for the field types (e.g., specify numbers for numeric fields).

If you select a URL that specifies a new value for a field, you must save the entity after opening the record in order to save the changes.

#record-manager/asset/<EntityKey>: Opens the Record Manager page for a record found in the asset hierarchy.
asset Specifies that the record you want to open in Record Manager is found in a family used in the asset hierarchy.asset

N/A

Entity KeySpecifies the Entity Key of the record that you want to open in the Record Manager.Any Entity Key that corresponds to an existing record in a family that appears in the asset hierarchy.

N/A

#bdf-screen/id/<datasheet ID>?familykey=<family key or id>&keys=<entity key 1>,<entity key 2>: Opens the Bulk Data Form for the specified entity keys using the desired datasheet.

#bdf-screen/id/<datasheet ID>?familykey=<family key or id>: Opens the Bulk Data Form for a new entity of the specified family using the desired datasheet.

#bdf-screen?familykey=<family key or id>&keys=<entity key1 >,<entity key 2>: Opens the Bulk Data Form for the specified entity keys.

#bdf-screen?familykey=<family key or id>: Opens the Bulk Data Form for a new entity of the specified family.

Family KeySpecifies the Family Key of the record that you want to open in the Bulk Data Form.Any Family Key that corresponds to a family.N/A
Family IDSpecifies the family ID of the record that you want to open in the Bulk Data Form.Alphanumeric Family IDThe Family ID parameter provides the same functionality as the Family Key parameter. In each URL that contains the Entity Key parameter, you can use either the Family Key or Family ID parameter. You do not need to use both.
Entity KeySpecifies the Entity Key of the record that you want to open in the Bulk Data FormAny Entity Key that corresponds to an existing record in a family that appears in the asset hierarchy.N/A
Datasheet IDSpecifies the datasheet that you want to display in the Bulk Data FormThe Datasheet ID of the desired datasheet.The Datasheet ID must correspond to a datasheet that has been defined for the specified family in the Configuration Manager. If you do not specify this parameter, the APM system will use the datasheet that the current user was last using when viewing a record in the specified family or the default datasheet if the user has never opened a record in that family before.
!datasheet-dialog/{family key or ID}/{entity key}?caption=<string>&canEdit=<true or false>&datasheetID={datasheet ID}&{field ID}=<string or [field ID]>: Opens the datasheet for an existing record in a separate window using the family key or ID.

!datasheet-dialog/{family key or ID}?caption=<string>&canEdit=<true or false>&datasheetID={datasheet ID}&{field ID}=<string or [field ID]>: Opens the datasheet for a new record in a separate window using the family key or ID.

Family Key

Specifies the Family Key of the record that you want to open in the Record Manager.

Any Family Key that corresponds to a family.N/A
Family IDSpecifies the family ID for a new record.Alphanumeric Family IDThe Family ID parameter provides the same functionality as the Family Key parameter. In each URL that contains the Entity Key parameter, you can use either the Family Key or Family ID parameter. You do not need to use both.
Entity KeySpecifies the Entity Key of the record that you want to open in the Record Manager.Any Entity Key that corresponds to an existing record in the specified family.

If you specify 0 or omit the entity key, a new record is created.

captionSets the title of the window.Any alphanumeric valueThis parameter is optional. If a title is not specified, the window title will appear as “Datasheet”.
canEditSets whether the Edit button appears in the window.Boolean valueThis parameter is optional. If this parameter is not specified, the value is assumed to be true; that is, the datasheet can be edited.
datasheetIDSpecifies the datasheet to display.Any Datasheet ID for the Family specified in the route.This parameter is optional. If this parameter is not specified, or is invalid, the user’s preferred datasheet is displayed.
Field IDSpecifies the ID of a field to be updated to a new valueAny valid value for the field, or, the ID of another field that contains a valid value for the field.This parameter is optional. Note that when you open the record in the new window, the updated values specified in the URL are not yet saved. You must save the record to accept the changes.

Example URLs

Example URLDestination
#record-manager/9876543/1234567 Opens the Record Manager, displaying the record with the Entity Key 1234567 and with the Family Key 9876543.
#record-manager/1234567 Opens the Record Manager, displaying a new record for the family with the Family Key 1234567.
#record-manager/Pump Opens the Record Manager, displaying a new record for the Pump family.
#record-manager/9876543/1234567?datasheetid=Custom_Datasheet Opens the Record Manager, displaying the record with the Entity Key 1234567 and Family Key 9876543. The datasheet Custom_Datasheet is selected by default.
#record-manager/1234567?Asset_Manf_CHR=Pacific Opens the Record Manager, displaying a blank record for the family with the Family Key 1234567. The field with the ID Asset_Manf_CHR is populated automatically with the value Pacific.
#record-manager/asset/1234567Opens the Record Manager displaying a record with entity key 1234567 and which appears in the asset hierarchy.
#bdf-screen?familykey=6785746&keys=12345678, 98765432Opens the Bulk Data Form, displaying the records with Entity Keys 12345678 and 98765432. The Family Key is 6785746.
#bdf-screen/ID/MI_EQUIP000_MXMO?familykey=MI_EQUIP000&keys=12345678, 98765432Opens the Bulk Data Form, displaying the records with Entity Keys 12345678 and 98765432. Family Key is MI_EQUIP000 and Family ID is MI_EQUIP000_MXMO.
!datasheet-dialog/MI_TASKINSP/12345678?caption=Inspection Task&canEdit=false Opens a specified record in a separate window with the title "Inspection Task" and without the Edit button.
!datasheet-dialog/MI_EQUIP000/12345678?datasheetID=EHW_STATUSOpens the specified Equipment record in a separate window using the EHW Status datasheet.
!datasheet-dialog/MI_EQUIP000/12345678?MI_EQUIP000_EQUIP_ID_C=New ID&

MI_EQUIP000_EQUIP_SHRT_DESC_C=[MI_EQUIP000_EQUIP_ID_C]

Opens the specified Equipment record in a separate window and sets the value of the Equipment ID field to “New ID”, and the value of the Short Description field to the previous value of the Equipment ID field.

Site Filtering in Record Manager

When you open a record in Record Manager, the site to which the record is assigned is displayed in the Site field, as shown below.

The Site field is not displayed when you access a record in a family for which the site filtering is disabled.

When you create or edit a record in the Record Manager, you can modify the value of the Site field according to the site filtering constraints for the relevant families and your site assignment.

  • When you use the Add New Record option to create a new record linked to an existing record, and the family of the new record has site filtering enabled, the site of the new record is set automatically based on the site of the existing record.
  • When you open an existing record in Record Manager and use the Link Existing Record option, the Search window only displays the records that can be linked with the existing record according to the site filtering configuration of the relevant families.
    Note: In most cases, the Search window displays only records assigned to the same site as the record initially opened in Record Manager, and records assigned to the Global site.
  • If you are a Super User, when you open an existing record in Record Manager, you can use the Site fields to change the site of the record.