Upgrade
Upgrade the ServiceMax Adapters to ServiceMax UDLP V2.6.0
The following table outlines the steps that you must complete to upgrade this module to ServiceMax UDLP V2.6.0.
About This Task
These instructions assume that you have completed the steps for upgrading the basic system architecture.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Procedure
- Upgrade from ServiceMax UDLP V2.2.0 through Maximo UDLP V2.5.0
- On the APM Connect Server, run the third-party software batch file.
- On the APM Connect Server, update existing jobs.
Create a ServiceMax EAM System Record
You must configure an EAM System record to establish a connection between any EAM system and Essentials.
Procedure
Results
- An EAM system record is created for the EAM system that defines a connection with Essentials. The ID for this EAM record should now be used in the Name field of a Site Reference record.
- Linking an EAM system to an EAM System record enables the APM Connect Adapters to create Notifications against that EAM System.
Configure the ServiceMax Context File
This topic describes how to access and configure parameters in the context file.
About This Task
Before you can run a job, you must specify a set of connection parameters and corresponding values to establish connections between APM Connect components, Essentials, and ServiceMax. Each of these connections is used when executing a job, and they are required. The connections are established via context files.
Procedure
Interface Mode Selection | ||
---|---|---|
Parameter | Description | Default or Recommend Value |
LOAD_MERIDIUM_APM | Determines if data will be loaded into the Meridium database. | The default value is true. true: data will be loaded into the Meridium database. false: data will not be loaded into the Meridium database. |
LOAD_DIGITAL_APM | Determines if data will be loaded into the Predix database. | The default value is true. true: data will be loaded into the Predix database. false: data will not be loaded into the Predix database. |
CMMS_ID |
The CMMS ID used as the identifier for your ServiceMax System, taking the form <System ID>-<Client ID>. For example, if your System ID is D03 and your Client ID is 001, then your CMMS ID would be DO3-001. |
This value is required. Enter your unique value. |
SOURCE_SYSTEM_TYPE | Identifies the type of system connecting with Essentials. |
This value is required. You must enter the value SERVICEMAX. |
Intermediate Repository (IR) Connection Parameters | ||
Parameter | Description | Default or Recommended Value |
IR_HOST | IP address of the IR. | Enter the host name of the PostgreSQL server. If you installed APM Connect using the default settings, then the value is localhost. |
IR_PORT | Port number of the IR. | The default value is 5432. |
IR_DATABASE | Database in which the IR data is stored. | Enter a name for the IR database. This value will be used to create the IR database. |
IR_SCHEMA | The schema in which the IR database will be created. | The default value is public. |
IR_USER_ID | The IR user name. | Enter the user name for the PostgreSQL database. The default user name is postgres. |
IR_PASSWORD | The IR system password. | Enter the password for the PostgreSQL database that was created when running the installer. |
APM Connection Parameters | ||
Parameter | Description | Default or Recommend Value |
APM_API_APP_SERVER | The Essentials API application server name. | Enter the name of your Essentials API Server. |
APM_API_USE_SSL | Specifies whether the Essentials API application uses SSL. | The valid values are:
The default value is false. |
APM_APP_SERVER | The Essentials application server name. | Enter the name of your Essentials Server. |
APM_DATASOURCE | The Essentials data source to which the data will be exported. | Enter the name of your Essentials data source. |
APM_PASSWORD | The Essentials Framework password. | Enter your unique value. |
APM_USERID | The Essentials Framework User ID. | Enter your unique value. |
UNC_FILE_PATH | The path of the directory of the data loader file share. | Enter your unique value. |
ServiceMax Organization Information | ||
Parameter | Description | Default or Recommended Value |
CUSTOMER_NAME | The coded customer name. | Enter your unique value, which was provided at installation. |
ServiceMax Connection Parameters | ||
Parameter | Description | Default or Recommended Value |
SERVICEMAX_CLIENT_ID | ServiceMax client from which data will be extracted. | Enter your unique value. |
CLIENT_SECRET | The secret associated to the ServiceMax Client. | Enter your unique value. |
GRANT_TYPE | The value ServiceMax uses to grant access to the system. | The default value is password. |
SERVICEMAX_TOKEN_REQUEST_URL | IP address of the ServiceMax Server that provides security tokens to users. | Enter your unique value. |
USERNAME | ServiceMax system user ID. | Enter your unique value. |
PASSWORD | ServiceMax system password. | Enter your unique value. |
SERVICE_REQUEST_URL | The URL of the service that Essentials uses to create service requests in ServiceMax. | Enter your unique value. |
ROWS_TO_PROCESS | The number of assets to extract in each batch from ServiceMax. | The default value is 100. |
LANGUAGE | The ServiceMax code that represents the language. | Must be a single character. |
EXTRACT_NUM_PARALLEL_JOB | Determines the maximum number of background jobs allowed during execution. | The recommended value is 10. |
IR_LOAD_NUM_PARALLEL_JOBS | The maximum number of IR load jobs in a single extraction. | The recommended value is 30. |
MANUAL_RUN | Determines how the date parameters will be treated. | The default value is true. true: The dates specified in the context file will be used, and the dates of the last successful run stored in the database will not be updated. false: The date range used during the extraction will be the date of the last successful record, as stored in the database. Each time a Job is run successfully, the database is updated with those dates, and all subsequent runs will use the dates from the last successful record. |
File System Parameters | ||
Parameter | Description | Default or Recommended Value |
PLSERVICEMAX_INPUT | Path of the directory you created in which ServiceMax writes files. | Enter your unique value. |
PLSERVICEMAX_OUTPUT | Path of the directory where APM Connect will access the files written by ServiceMax. | Enter your unique value. |
IR_TALEND_OUTPUT | The root directory for all internal file processing. This is the directory where files will be transformed. | Enter a file system location to which files will be written. You can create a directory in the following location: C:\IR\TalendOutput. |
LOG_BASE_DIR | The directory path to the log file. | None. |
SFTP_STAGING_DIR | Temporary storage location for files that are waiting to be loaded. | Enter your unique value, which was provided at installation. |
USE_SSL | Determines if an SSL certificate will be used when transferring files. |
Enter true. An SSL certificate is required, and true is the only valid value. |
TRUSTSTORE_FILE | The directory path where the SSL certificate is stored. | Enter the directory path where the SSL truststore is stored on the APM Connect Server. |
TRUSTSTORE_PASSWORD | The password to the SSL certificate file. | Enter your unique value, which was provided at installation. |
Filter Parameters | ||
Parameter | Description | Recommended or Default Value |
CREATE_DATE_START | Date value that limits the data extracted to records created on or after the specified date. | Dates must be entered in the following format: YYYYMMDD. |
CREATE_DATE_END | Date value that limits the data extracted to records created on or before the specified date. | Dates must be entered in the following format: YYYYMMDD. |
CHANGE_DATE_START | Date value that limits the data extracted to records changed on or after the specified date. | Dates must be entered in the following format: YYYYMMDD. |
CHANGE_DATE_END | Date value that limits the data extracted to records changed on or before the specified date. | Dates must be entered in the following format: YYYYMMDD. |
CREATE_TIME_START | Time value that limits the data extracted to records created at or after the specified time. | Time must be in the following format: HHMMSS |
CREATE_TIME_END | Time value that limits the data extracted to records created at or before the specified time. | Time must be in the following format: HHMMSS. |
CHANGE_TIME_START | Time value that limits the data extracted to records changed at or after the specified time. | Time must be in the following format: HHMMSS. |
CHANGE_TIME_END | Time value that limits the data extracted to records changed at or before the specified time. | Time must be in the following format: HHMMSS. |
Equipment Filter Criteria | ||
Parameter | Description | Recommended or Default Value |
SERVICEMAX_MAX_ASSETID | Specifies the IDs of the assets that you want to extract. | Enter your unique value. Suppose that you want to extract assets between IDs 12345 and 98764. Your configuration would contain this statement:
|
SERVICE_MAX_WONUM | Specifies the Work Order numbers you want to extract. | Enter your unique value. Suppose you want to extract work orders between IDs 8756 and 9875. Your configuration would contain this statement:
|
SERVICE_MAX_SRNUM | Specifies the Service Request numbers you want to extract. | Enter your unique value. Suppose you want to extract service requests a2C1I000000F2y and b2C1I000000F2z. Your configuration would contain this statement:
Note: This filter will only extract service requests that do not have associated work orders. |
EQUIPMENT_NO | Equipment that you want to extract. | The Equipment number cannot exceed 18 characters. You cannot exceed 500 Equipment numbers. |
EQUIPMENT_CATEGORY | ID of the Equipment Category that will limit the Equipment extracted. | The Equipment Category cannot exceed one character. |
EQUIPMENT_TYPE | ID of the Equipment Type that will limit the Equipment extracted. | The Equipment Type cannot exceed 10 characters. |
EQUIPMENT_CLASS | ID of the Equipment Classification that will limit the Equipment extracted. | The Equipment Class cannot exceed 18 characters. If an Equipment has multiple classifications, as long as you specify one of those classifications, the Equipment record will be extracted. |
Predix Parameters | ||
Parameter | Description | Recommendation or Default Value |
TOKEN_REQUEST_URL | The URL of the service that issues tokens for a client. | Enter your unique value. |
CLIENT_ID | The client ID to access the Predix application. | Enter your unique value. |
INGESTION_USERNAME | The user name to request asset data from the Predix application. | Enter your unique value. |
INGESTION_PASSWORD | The password for the ingestion user name that requests asset data from the Predix application. | Enter your unique value. |
ASSET_INGESTION_URL | The URL the Predix application uses to respond to requests for asset information. | Enter your unique value. |
TENANT_UUID | The userid of the tenant used to access the Predix application. | Enter your unique value. |
PREDIX_GRANT_TYPE | The value the Predix application uses to grant access to the system. | The default value is password. |
Functional Location Filter Criteria | ||
Parameter | Description | Recommended or Default Value |
FLOC_NO | ID of the Functional Location that will limit the Functional Locations extracted. | The Functional Location number cannot exceed 40 characters. You cannot exceed 500 Functional Location numbers. |
FLOC_TYPE | ID of the Functional Location Type that will limit the Functional Locations extracted. | Functional Location type cannot exceed 10 characters. |
FLOC_CLASS | ID of the Functional Location Classification that will limit the Functional Locations extracted. | Functional Location class cannot exceed 18 characters. |
FLOC_CATEGORY | ID of the Functional Location Category that will limit the Functional Locations extracted. | Functional Location category cannot exceed one character. |
Work History Filter Criteria | ||
Parameter | Description | Recommended or Default Value |
NOTIFICATION_NO | Number that identifies the Notification record. | Notification Number cannot exceed 12 characters. |
WORK_ORDER_NO | Number that identifies the Work Order record. | Work Order Number cannot exceed 12 characters. |
NOTIFICATION_TYPE | Order type that limits the orders that you want to extract. | Notification type cannot exceed two characters. |
WORK_ORDER_TYPE | ID of the work order that limits the orders that you want to extract. | Work Order type cannot exceed four characters. |
WORK_ORDER_SYSTEM_STATUS | Work Order systems status that limits the work orders you want to extract. | Work Order System Status cannot exceed four characters. |
WORK_ORDER_USER_STATUS | Work Order user status that limits the work orders that you want to extract. | Work Order User Status cannot exceed four characters. |
NOTIFICATION_SYSTEM_STATUS | Notification system status that limits the notifications that you want to extract. | Notification system status cannot exceed four characters. |
NOTIFICATION_USER_STATUS | Notification user status that limits the notifications that you want to extract. | User status cannot exceed four characters. |
MAINT_PLANT | ID(s) of the Maintenance Plant whose data you want to extract. | Plant values cannot exceed four characters. |
Miscellaneous Parameters | ||
Parameter | Description | Recommended or Default Value |
SITE_REFERENCE_EQUIP | Used to map the site reference value to a ServiceMax field. This dictates which ServiceMax field will be used as the site reference for Essentials Equipment records. | You can enter a value defined in Essentials. Note: The value that is entered will be applied to all records. -or- You can use the character # at the beginning and end of a Essentials field name to indicate the field that is used to set the site reference. For example, if you wanted to use your ServiceMax maintenance plant field as your Essentials site reference, you would enter a value in the following form: <SITE_REFERENCE_EQUIP>#MI_EQUIP000_MAINT_PLANT_C#</SITE_REFERENCE_EQUIP>. |
SITE_REFERENCE_FLOC | Used to map the site reference value to a ServiceMax field. This dictates which ServiceMax field will be used as the site reference for Essentials Equipment records. | Specify the value with either of the following methods:
For example, if you wanted to use your ServiceMax maintenance plant field as your Essentials site reference, you would enter a value in the following form: <SITE_REFERENCE_FLOC>#MI_FNCLOC00_MAINT_PLANT_C#</SITE_REFERENCE_FLOC>. |
Email Notification Parameters | ||
Parameter | Description | Recommenced or Default Value |
EMAIL_TO | The email address(es) to which the notification email will be sent. | Enter your unique value. |
EMAIL_FROM | The email address from which the notification email will be sent. | Enter your unique value. |
REPORT_TARGET_DIR | The directory path where the report file will be delivered. | Enter your unique value. |
FAILURE_DETAIL_REPORT_JRXML_FILE_PATH | The directory path where the failure report file will be delivered. | Enter your unique value. |
LOAD_SUMMARY_REPORT_JRXML_FILE_PATH | The directory path where the load complete report file will be delivered. | Enter your unique value. |
SMTP_HOST | The SMTP host for the APM Connect Server installation. | Enter your unique value. |
SMTP_PORT | The port for SMTP. | Default value is 25. |
LOAD_SUMMARY_REPORT_ENABLED | Indicates whether the Load Complete report will be sent with every extraction. |
True: The Load Complete report will be sent detailing the number of records that were extracted and successfully loaded into Essentials. False: The Load Complete report will not be sent. |
FAILURE_DETAIL_REPORT_ENABLED | Indicates whether the Failure Detail report will be sent when a record fails to load. |
True : The Failure Detail report will be sent detailing the records that failed to load and the reason why. False: The Failure Detail report will not be sent. |
Configure Site Reference Values
To assign site references to records using values other than those in the baseline configuration, you must modify the autojoin_control table in the Intermediate Repository.
About This Task
Procedure
- Configure the Site Reference Value to Use an Indirect Site Reference Value.
- Configure the Site Reference Value to be A Specific Site Name.
Example: Configure MI_EQUIP000_CST_CNR_C as an Indirect Site Reference
In this example, the database browser tool used in this example is pgAdmin4, the IR database name is ServiceMax_UDLP_EAMClient. You can use the database browser of your choice.
- On your APM Connect Server, open the application pgAdmin4.
The application pgAdmin4 opens, displaying your available servers.
- Navigate the server tree to the appropriate IR database, access your tables.
In this example, the path is Servers(2)\roaperflabvm3\Databases\ServiceMax_UDLP_EAMClient\Schemas(1)\public\Tables (81). The list of tables in your IR database are visible.
- Locate the table autojoin_control, then right-click the table, and then select View Data.
- Select View All Rows.
The Query -1 section is populated with the autojoin table.
- In each row, in the site_reference column, enter
#MI_EQUIP000_CST_CNR_C#
Tip: This example assumes that the existing values in the site_reference column correspond to values in the MI_EQUIP000 and MI_FNCLOC00 families. If they do not, you must also update the apm_site_reference_family column to the corresponding family.The value in the MI_EQUIP000_CST_CNR_C field will be used to populate the Site Reference Key in corresponding records.
Create Notifications Recommendation Records
ServiceMax allows you to create Recommendation records in Essentials that will be used to create ServiceMax Notifications automatically. You can configure Essentials to create Notifications Recommendation Records.
About This Task
For a Recommendation record to generate an ServiceMax Notification automatically, the Create Work Request field must exist on the Recommendation datasheet. This field is available on the baseline datasheets for the baseline Recommendation families from which you can create ServiceMax Notifications.
If you want to generate ServiceMax Notifications from Recommendation records that belong to customer-defined subfamilies of the root Recommendation family, in addition to implementing the correct rules (for an example of the rules that you will need to implement, you can look at any active baseline Recommendation family), you will need to add the Create Work Request field to the applicable datasheets for that family.
Procedure
- Add the Notification Type field to the datasheet.
- Configure the Notification Type field to accept values other than general. Note: In the baseline ServiceMax product, this field is disabled. If desired, you could configure it to be enabled so that users can enter a value directly in the Notification Type cell on the datasheet. You might also consider creating a Valid Values rule that provides a list of acceptable values so that users can select the desired value in the list.
Enable ServiceMax and APM Connect Communications
To enable communications between ServiceMax and APM Connect, the ServiceMax administrator must update ServiceMax correctly. To configure communications, you must provide the ServiceMax administrator with specific information.
Provide the ServiceMax administrator with the userid configured in the context file as USERNAME for APM Connect.
Provide the ServiceMax administrator with the following information:
-
The EVENT NAME and CLASS NAME are APMServiceRequestEvent. The administrator will configure these values in the IoT Events section on the IoT Setup page in ServiceMax.
- The INSTALLED PRODUCT FIELD NAME is Record ID and the EXTERNAL FIELD NAME is RecordID. The administrator will configure these values in the Installed Product Lookup section in the IoT Setup page in ServiceMax.