Review Deployments

Review Deployment Configuration

Use the Review step to access, modify, and deploy your selections.

Before You Begin

Make sure you have completed the first three steps of deployment.

About This Task

Each subsection in the Review section includes information about your deployment configuration efforts. After completing all the required configuration modifications, you can deploy the analytic to the respective runtime environment, and run it at the scheduled time.

Procedure

  1. In the Applications menu, navigate to RELIABILITY > Analytics > Deployments.
  2. In the Search pane, select an existing deployment to access its workspace.
  3. In the page header, select Edit to access the 1. Asset Selection section.
  4. Select the 4. Review tab.
  5. Make the required modifications to relevant subsections of the page. Do one or more of the following:
    • Make required modifications, then select Save in the step before proceeding to the next step.
    • Select Next to proceed to the next section without modifying the current section.
    After modifying the required subsections, return to the 4. Review section when you are done.
  6. Select Deploy to upload the deployment to the runtime and run the analytic.
    When you select Deploy or Close, you are returned to the Deployments details page.