Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / AlarmQueryResponseHandler Delegate
Whether this is the final response.
The returned list of alarms or events.
The number or alarms or events returned.


AlarmQueryResponseHandler Delegate
A delegate invoked for Alarm/Events Query Response.
Syntax
Public Delegate Sub AlarmQueryResponseHandler( _
   ByVal final As System.Boolean, _
   ByVal alarmNotificationInfo As AlarmNotificationInfo, _
   ByVal numAlarms As System.Integer _
) 

Parameters

final
Whether this is the final response.
alarmNotificationInfo
The returned list of alarms or events.
numAlarms
The number or alarms or events returned.
Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also