Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / Field Class
Members


Field Class
This represents the individual field within the MultiField class.
Syntax
Public Class Field 
Inheritance Hierarchy

System.Object
   Proficy.Historian.ClientAccess.API.Field

Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also