Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / ArrayValue Class
Members


ArrayValue Class
This is the value type for array tags in Historian
Syntax
Public Class ArrayValue 
Inheritance Hierarchy

System.Object
   Proficy.Historian.ClientAccess.API.ArrayValue

Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also