Method Reference M-P
- M
- ManageServerDialog Method (ServerManager Object)
-
Displays a window to manage server connection information on the client. This window allows you to add and remove new connections, and to modify the default username and password. This method optionally returns the name of the server last selected in the window.
Syntax
object.ManageServerDialog([SelectedServer])Table 1. Parameters Name Data Type Description SelectedServer String Name of the selected Historian Server (optional, read/write). Returns
None.
ExampleDim MyManager As New iHistorian_SDK.ServerManager Dim MyServer As iHistorian_SDK.Server Dim SelectedServer As String ' Show the manage server window MyManager.ManageServerDialog SelectedServer ' If a server was selected, get the server If Trim(SelectedServer) <> "" Then Set MyServer = MyManager.Servers(SelectedServer) End If - N
- NewRecordset Method (Data Object)
-
Returns a new DataRecordset object to subsequently build a query for tag data from the Historian server. It is the responsibility of the developer to release the DataRecordset object when processing has been completed. DataRecordset objects may be re-used by re-executing a query with new criteria set through the DataCriteria of the DataRecordset object.
You must also use a new DataRecordset object to add new data points to the system and delete existing data points from the system. Changes are not committed until calling the WriteRecordset method of the DataRecordset object.
Syntax
object.NewRecordset
Parameters
None
Returns
DataRecordset. A new, empty, DataRecordset object.
- NewRecordset Method (Messages Object)
-
Returns a new MessageRecordset object to build a query for messages and alerts from the Historian server message archive. You must release the MessageRecordset object when processing completes. You can re-use a MessageRecordset object by re-executing a query with new criteria set through the MessageCriteria of the MessageRecordset object.
To add new messages, you must use a new MessageRecordset object. Call the WriteRecordset method of the MessageRecordset object to commit changes to the archiver.
Syntax
object.NewRecordset
Parameters
None
Returns
MessageRecordset. Returns the newly created MessageRecordset object.
- NewRecordset Method (Tags Object)
-
Returns a new TagRecordset object to build a query for tag information. You must terminate the TagRecordset object when processing completes. You can re-use the TagRecordset objects by re-executing a query with new criteria set through the TagCriteria of the TagRecordset object.
You must also use a new TagRecordset object to add new tags to the system and to delete tags from the system. Call the WriteRecordset Method of the TagRecordset object to commit changes to the archiver.
Syntax
object.NewRecordset
Parameters
None.
Returns
TagRecordset. Returns a reference to the newly created Recordset Object.
- Purge Alarms By Id Method
Purges a single alarm as identified by its alarm ID.
Syntax
object.AlarmIdsTable 2. Parameters Name Data Type Description AlarmIds Long Alarm ID of the alarm. Returns
Boolean. Returns TRUE if the alarm is purged.
Example
Dim Status As ihStatus Dim ReturnStatus As Boolean Dim Alarms() As Long Dim NumberOfAlarms As Long Dim i As Long Status = ihSTATUS_FAILED ReturnStatus = False NumberOfAlarms = (UBound(AlarmIds) + 1) ReDim Alarms(0 To NumberOfAlarms - 1) As Long On Error GoTo errc For i = 0 To NumberOfAlarms - 1 Alarms(i) = AlarmIds(i) Next i Status = ihPurgeAlarmsById(MyServer.Handle, Alarms(0), NumberOfAlarms, 0) If Status <> ihSTATUS_OK Then err.Raise 1, , "Error Purging alarms by Id[" + ErrorDescription(Status) + "," + CS ReturnStatus = True PurgeAlarmsById = ReturnStatus errc: zLastError = "Purge Alarms By Id>> " + err.Description PurgeAlarmsById = ReturnStatus End Function- Purge Alarms Method
-
Purges or deletes the alarms from the Archiver.
Syntax
object.PurgeAlarms
Table 3. Parameters Name Data Type Description BackupFile String The file that stores the purged alarm data. ShouldZipAlarms Boolean Indicates whether the alarms should be zipped into file or not. StartTime Date Start time of the alarms. EndTime Date End time of the alarms. Returns
Boolean. Returns TRUE if the alarms are purged.
Example
Dim Status As ihStatus Dim AlarmsStartTime As ihTimeStruct Dim AlarmsEndTime As ihTimeStruct Dim ShouldZip As ihBoolean Dim ReturnStatus As Boolean Status = ihSTATUS_FAILED ReturnStatus = False AlarmsStartTime = Date_To_UTC(StartTime) AlarmsEndTime = Date_To_UTC(EndTime) If ShouldZipAlarms = True Then ShouldZip = ihTRUE Else ShouldZip = ihFALSE End If On Error GoTo errc Status = ihPurgeAlarms(MyServer.Handle, BackupFile, ShouldZip, AlarmsStartTime, AlarmsEndTime, 0) If Status <> ihSTATUS_OK Then err.Raise 1, , "Error Purging alarms [" + ErrorDescription(Status) + "," + CStr(St ReturnStatus = True PurgeAlarms = ReturnStatus errc: zLastError = "Purge Alarms>> " + err.Description PurgeAlarms = ReturnStatus End Function