Add Degradation Mechanisms (DMs)

Note: You cannot add a DM if the state of the analysis is Risk Completed.

Steps

  1. Access the analysis to which you want to add DMs.
  2. In the workspace heading, select the Degradation Mechanisms tab.

    The Degradation Mechanisms section appears, displaying a list of DMs associated with the analysis.

  3. In the Degradation Mechanisms section, select .

    A list of the DMs that can be applied to the RBI Criticality Analysis appears.

  4. Next to the DMs you want to add, select the check boxes.
  5. Select Add.

    The selected DMs are added to the RBI Criticality Analysis.