Calculate all RBI Criticality Analyses Associated with Multiple Assets

You can also calculate:

Steps

  1. Access the Risk Based Inspection Overview page for the Functional Location that contains the assets for which you want to calculate all analyses.

  2. If you want to calculate analyses associated with all the assets in the functional location, then proceed to step 5. You cannot, however, calculate all analyses if you have selected Home on the Asset Hierarchy page.
  3. If you want to calculate analyses associated with selected assets, then in the workspace heading, select the Assets tab.

    The Assets section appears.

  4. Select the check boxes that correspond to the assets for which you want to calculate all analyses.

  5. In the upper-right corner of the page, select .

    Note: If you have selected Home on the Asset Hierarchy page, and have not selected any assets, then the button is disabled.

    A message appears, specifying the number of assets that you have selected, and asking you if you want to continue.

  6. Select Yes.

    The Calculate Analysis window appears, displaying a list of analyses that are sent for calculation, the asset and the component that each analysis is associated with, and the status of each calculation.

    If the calculation fails, a list of the required fields appear in an error report at the bottom of the Calculate Analysis window.

  7. If you want to view the log of a particular calculation or validation, select the analysis in the list.

    A log of the calculation or validation associated with the selected analysis appears, which includes error messages, if any.

  8. If you want to view the log of all the calculations, select View Complete Log.
  9. If you want to close the window, select Close.

    If the calculations are not yet complete, then a message appears, stating that the details of the calculation will no longer be available.

  10. Select Yes.

    The Risk Based Inspection Overview page appears. You can continue using Meridium Enterprise APM. If you want to check the check the status of the bulk calculation, then in the upper-right corner of the page, select .