This topic describes how to calculate multiple RBI Analyses associated with a single Asset or Corrosion Loop.
You can also calculate:
Steps
Access the Risk Based Inspection Overview page for the Functional Location that contains the asset for which you want to calculate multiple analyses.
Note: You can also access a Corrosion Loop and proceed to step 4.
In the workspace heading, select the Assets tab.
The Assets section appears.
In the Assets section, select the Asset ID that corresponds to the asset for which you want to calculate multiple analyses.
The Asset Summary workspace appears, displaying the Asset Overview section.
Note: You will only see graphs representing RBI 581 Risk Analyses and RBI Criticality Analyses side-by-side if you have both the Risk Based Inspection and RBI 581 modules active at the same time. Otherwise, depending on which module is active, only the corresponding graph appears.
In the workspace heading, select
The Calculate Analysis window appears, displaying a list of analyses that will be calculated and a log.
If the calculation fails, a list of the required fields appear in an error report at the bottom of the Calculate Analysis window.
In the list, select the analysis whose log you want to view.
A log of the operation associated with that analysis appears, along with an explanation of any errors.