Note: The Risk Analysis Mapping family supports RBI Criticality, RBI Pipeline, and RBI PRD Criticality Analyses. These mappings support both the default and Standard Practice Risk Matrix.
The Risk Analysis Mapping family defines the Policy records that are used to populate the RBI Risk Matrix automatically from RBI Analyses. The information in the following table reflects the baseline state and behavior of fields that exist in the Risk Analysis family.
Field | Caption | Data Type | Description | Behavior and Usage |
---|---|---|---|---|
MI_RRSKMAP_ANLY_FAM_C | Analysis Family | Character | The Family ID of the analysis. | This field is populated by default in each Risk Analysis Mapping record that is delivered to the baseline Meridium Enterprise APM database. |
MI_RRSKMAP_DEG_MECH_C | Degradation Mechanism | Character | The Degradation Mechanism that stores values that will be used to populate the Risk Matrix. | This field is populated by default in each Risk Analysis Mapping record that is delivered to the baseline Meridium Enterprise APM database. |
MI_RRSKMAP_POLICY_NM_C |
Policy Name | Character | The name of the Policy that will be used to populate the Risk Matrix. | This field is populated by default in each Risk Analysis Mapping record that is delivered to the baseline Meridium Enterprise APM database. |
MI_RRSKMAP_RISK_CTG_C | Risk Category | Character | The Risk Category that will be populated on the Risk Matrix (Environment, Financial Risk, Operations, Safety). | This field is populated by default in each Risk Analysis Mapping record that is delivered to the baseline Meridium Enterprise APM database. |
The Policy Input Nodes that are used by the Risk Analysis Mapping family to populate the RBI Risk Matrix depend on both the type of Risk Category that you choose and the Degradation Mechanism that you apply to the family. The information in the following tables indicates which policy nodes and input fields will be used when populating your selected RBI Risk Matrix.
Note: When running a RBI 580, PRD, or Pipeline Analysis, the Failure Frequency field is populated by Degradation Mechanism Evaluation respective to each Degradation Mechanism in selected RBI Analysis.