Access the RCA Overview Page for all Asset Hierarchy Levels

This topic describes how to access the RCA Overview page on which you can view all the information and perform various tasks related to root cause analyses for various Asset Hierarchy Levels. If you want to view root cause analyses associated with a particular Asset Hierarchy Level, you can access the RCA Overview page for an Asset Hierarchy Level.

You can perform various tasks on this page based on the membership in various Security Groups.

Steps

  1. On the Meridium navigation menu, select Performance, and then select Root Cause Analysis.

    The RCA Overview page appears, displaying the following information related to the root cause analyses for all Hierarchy Levels:

    RCA Overview

    While viewing any of the above graphs, you can select to customize the appearance of the graph.

    By default, the hierarchy level is set to Home. You can filter the hierarchy level by selecting in the upper-left corner of the page.

    By default, the Root Cause Analysis information on this page is related to an Asset and children of the Asset. If you also want to view Root Cause Analysis information that is not related to an Asset, in the Include analyses without any assets? box, select Yes.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.