The following table lists the name and description of the subreports that are used to generate the Comprehensive Analysis Report, any queries that support the subreports, and the Comprehensive Analysis Report sections that the subreports and supporting queries are used to generate.
SubReport Name | Supporting Query | Behavior and Usage | Comprehensive Analysis Report Section |
---|---|---|---|
AAAGPage |
None |
Provides an introduction to the PROACT RCA Analysis-At-A-Glance Overview section. |
|
AAAGReview |
|
Provides a summary of the RCA, which includes data such as the name of the RCA, the name of the Principal Analyst, the start date, and the estimated completion date. |
|
AnalzyePage |
None |
Provides information about the Analyze step of a Root Cause Analysis. |
|
CommunicatePage |
None |
Provides information about the Communicate step of a Root Cause Analysis. |
|
Comprehensive Report |
None |
Provides necessary input for the Comprehensive Analysis Report. |
None |
Cover |
Cover Query |
Provides basic analysis information, such as the Analysis Name, Principal Analyst, and the date on which the report was generated. |
|
CSF |
CSF Query |
Provides a list of the Critical Success Factors that are defined for the RCA. |
|
CSFMain |
CSF Query |
Provides the charter and the Critical Success Factors that are defined for the RCA. |
|
DataCollection |
DataCollection Query |
Provides a list of the RCA Preserve Items that are included in the RCA. |
|
DataCollectionFileLink |
DataCollectionFileLink Query |
Provides a list of the RCA Preserve Items that are included in the RCA. |
|
EventDiagram |
EventDiagramImage Query |
Provides an image of the Event Diagram that exists for the RCA |
|
EventSummary |
None |
Provides information stored in the Event Narrative and the Mechanism fields of the Root Cause analysis. |
|
LogicTree |
LogicTreeImage Query |
Provides an image of the Logic Tree that exists for the RCA. |
|
OrderPage |
None |
Provides information about the Order step of a Root Cause Analysis. |
|
PreservePage |
None |
Provides information about the Preserve step of a Root Cause Analysis. |
|
RecommendationFileLinks |
RecommendationFileLinks Query |
Provides a list of the Reference Documents that are linked to the RCA Recommendations that are included in the RCA. |
|
RecommendationSummary |
None |
Provides a list of the RCA Recommendations that are included in the RCA. |
|
TableOfContent |
None |
Provides a list of the titles of the sections that are included in the Comprehensive Analysis Report. |
|
TeamMemberPrincipal |
TeamMemberPrincipal Query |
Identifies the Principal Analyst and identifying information from the associated Human Resource (e.g., name and contact information). |
|
TeamMembers |
TeamMember Query |
Provides a list of the team members who belong to the RCA Team, including various identifying information from the associated Human Resources (e.g., name and contact information). |
|
TrackingSummary |
Tracking Query |
Provides information from the RCA Tracking Items that are linked to the RCA. |
|
TrackPage |
None |
Provides information about the Track step of a Root Cause Analysis. |
|
VerificationFileLinks |
VerificationFileLink Query |
Provides a list of the Reference Documents that are linked to the RCA Verifications that are included in the RCA. |
|
VerificationLogs |
Verification Query |
Provides a list of the RCA Verifications that are included in the RCA. |
Each supporting query that is listed in this table contains a prompt on the ENTY_KEY field of the RCA family. When you run a report from the Reports List page, the ENTY_KEY of the RCA associated with the current RCA is passed automatically to the prompt. After the ENTY_KEY is passed, the results for the current RCA are displayed. If you run an RCA report or query from the Catalog, however, you will need to supply the ENTY_KEY for an RCA manually to retrieve results.
Copyright © 1993-2016 Meridium, Inc. All rights reserved.