Copy a System/Node

This topic describes how to copy a System/Node. You can also create a new System/Node. When you copy a System/Node, the related Deviations or What Ifs, Causes, Consequences, Safeguards, and Risk Assessments are also copied and associated with the copy of the System/Node.

Hint: You can copy a System/Node only if the Hazards Analysis into which you want to copy the System/Node is in the Planning state.

Note: When you copy a System/Node, the linked assets are not copied.

Steps

  1. Access the Hazards Analysis to which you want to copy the System/Node.
  2. In the left pane, select , and then select Copy.

    The Search window appears.

    The Search window

  3. In the upper-right corner of the window, select .

    A list of Systems/Nodes appears.

    The Search window

  4. Select the System/Node that you want to copy, and then select OK.

    A copy of the System/Node is created and associated with the Hazards Analysis. All related Deviations or What Ifs, Causes, Consequences, Safeguards, and Risk Assessments are also copied and associated with the copy of the System/Node.

What's Next?

Copyright © 2017 General Electric Company. All rights reserved.