Use Cases
The Common components include Configuration Hub and Proficy Authentication elements. Install these components from the MQTT Client 2024 Proficy installer welcome screen once on your machine within the same network. The Common components serve as shared centralized services for the MQTT Client product.
The following scenarios guide you in choosing the appropriate registration methods for MQTT Client installed before or after upgrading common components to version 2024 or higher.
Use case 1
First time Install: MQTT Client and Common components (Version 2024 or
higher)
Scenario | Tasks to Perform |
---|---|
Common components installed before MQTT Client installation. | Perform Install Time Registration for MQTT Client during the MQTT
Client installation. Note: If you skip providing
Configuration Hub and Proficy Authentication details during Install Time
Registration method, then perform Central Registration for MQTT Client method after MQTT Client installation. |
Common components installed after MQTT Client installation. | Perform Central Registration for MQTT Client after MQTT Client installation. |
Use case 2
MQTT Client Upgrade from Version 2023 to 2024 or higher version
Scenario | Tasks to Perform |
---|---|
Common components already upgraded to version 2024 or higher. | Perform Install Time Registration for MQTT Client during the MQTT
Client upgrade. Note: If you skip providing Configuration Hub
and Proficy Authentication details during the Install Time Registration method,
then perform Central Registration for MQTT Client method after the
MQTT Client upgrade. |
Common components are installed later with version 2024 or higher. | Perform Central Registration for MQTT Client after upgrading MQTT Client. |
Common components installed but not upgraded to version 2024 or higher. |
Important:
Upgrade common components to version
2024 or higher. |
Use case 3
MQTT Client Unregistration
Scenario | Tasks to Perform |
---|---|
MQTT Client registered with version 2024 common components or higher. | Unregister MQTT Client centrally from Configuration Hub. |
MQTT Client of version 2023 (registered conventionally) to common components of version 2024 or higher. | Unregister MQTT Client conventionally. |
Use case 4
Pre-2024 MQTT Client Registration
Scenario | Tasks to Perform |
---|---|
MQTT Client registration and unregistration before version 2024 with common components of version 2024 or higher. | Follow the conventional process for registration and unregistration. |
Use case 5
Migration of Common Components (Version 2024 or later)
Post-Registration
Scenario | Tasks to Perform |
---|---|
If you migrate to a new Proficy Authentication server. |
|
If you migrate to a new Configuration Hub server. |
|
If you migrate both the new Configuration Hub server and the Proficy Authentication server. |
|